Real Time

Channel Setup – Advanced Downlink Carrier

Advanced downlink carriers consist of the following:

This topic describes the parameters available in the advanced downlink Closedchannel setup node.

Channel Configuration Summary Table

This table enables you to view the key parameters for each channel in a carrier. All of the advanced downlink carrier channel configurations (RMC/RMC+HSET) are created in accordance with the 3GPP standards.

This button opens a window of predefined channel configuration selections according to the selected carrier type:

Double-clicking a configuration or clicking OK replaces the current configuration in the setup table. Select the carrier type from the Waveform or Carrier views.

This button opens a Closeddrop-down menu for selecting a channel to add to the setup table. The channel is inserted above the currently highlighted channel in the table.

for Adv W-CDMA/HSDPA DL Rel 6


for Adv W-CDMA/HSPA+ DL Rel 10

This button deletes the currently highlighted channels in the setup table. You can highlight multiple channels by holding down the CTRL key while selecting the channels. You can also use the SHIFT key to select a succession (group) of channels.

This button is only available for Adv W-CDMA/HSPA+ DL Carrier Rel 10. You can normalize power (relative power) to make the total power 0dB.

Channel List and Parameters

The following lists show the available channels for the advanced downlink carrier. Click on the channel of interest to view its parameters with links to their descriptions:

 

3GPP

Absolute Grant Scope

Range: 0, 1

Default: 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0

For the E-AGCH channel, this cell sets the Absolute Grant Scope pattern.

Absolute Grant Value

Range: 0, 1, 2, ..., 31

Default: 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0

For the E-AGCH channel, this cell sets the Absolute Grant Value pattern.

For the Absolute Grant Scope and Absolute Grant Value, users must input the value for each sub frame and separate the values with commas.

Take 4 frames (20 sub frames) for example, the input values are 1,1,1,1,1,1,1,1,1,1,1,1,1,1,1,1,1,1,1,1.

If the E-DCH TTI is 10ms, users can set the values in one frame to be the same. For example, the input values of Absolute Grant Scope are 1,1,1,1,1,0,0,0,0,0,1,1,1,1,1,0,0,0,0,0.

Alternative UE ID

Range: 0 to 65535

Default: 65535

For the HS-SCCH channel, this cell sets the identity of the UE different from the UE under test.

ARQ Type

Choices: NONE | HARQ

Default: HARQ

Double-click or use the drop-down menu to select the ARQ Type. This setting is available on the HS-PDSCH with the HSDSCH data selection and available on the HS-SCCH with the STD data selection.

NONE

HARQ settings are inactive (greyed out) and ignored by the software

HARQ

HARQ settings are active:

Because the HS-SCCH uses the HARQ setting in its coding, it is always available on this channel with the STD data selection. However if the HS-DSCH is not the HS-PDSCH data type, the HS-PDSCH does not broadcast the HARQ even if the HS-SCCH setting is HARQ.

This setting is coupled between the HS-SCCH and the HS-PDSCH so that if it is set on one channel, it also changes the setting on the other channel.

BCH Block Size

For the P-CCPCH channel, this cell only provides information (not editable) on the BCH block size in the current predefined channel configuration, which complies with the 3GPP standards. The information in this cell is fixed, and only visible and relevant when BCH is the data selection for the Data cell.

BCH Coding Type

For the P-CCPCH channel, this cell only provides information (not editable) on the BCH coding type in the current predefined channel configuration, which complies with the 3GPP standards. The information in this cell is fixed, and only visible and relevant when BCH is the data selection for the Data cell.

BCH CRC

For the P-CCPCH channel, this cell only provides information (not editable) on the BCH cyclic redundancy bits in the current predefined channel configuration, which complies with the 3GPP standards. The information in this cell is fixed, and only visible and relevant when BCH is the data selection for the Data cell.

BCH Data

Choices: PN9 | PN15 | BCCH-BCH-Message| User Defined Bits

Default: BCCH-BCH-Message

This cell is available only when BCH is the current data selection for the P-CCPCH.

For the P-CCPCH channel type, when you click the cell, a dialog box button ( ) appears and provides access to Data Source Selection dialog box where you select the data type.

BCH Number of Blocks

For the P-CCPCH channel, this cell only provides information (not editable) on the BCH number of blocks in the current predefined channel configuration, which complies with the 3GPP standards. The information in this cell is fixed, and only visible and relevant when BCH is the data selection for the Data cell.

BCH Rate Matching Attribute

For the P-CCPCH channel, this cell only provides information (not editable) on the BCH rate matching attribute in the current predefined channel configuration, which complies with the 3GPP standards. The information in this cell is fixed, and only visible and relevant when BCH is the data selection for the Data cell.

BCH TTI

For the P-CCPCH channel, this cell only provides information (not editable) on the BCH TTI in the current predefined channel configuration, which complies with the 3GPP standards. The information in this cell is fixed, and only visible and relevant when BCH is the data selection for the Data cell.

Block Number of Max TF

Range: 0 to 512

The behavior of this parameter is dependent upon the Transport Position selection.

Fixed Transport Position

This sets the block number of the TF which has the maximum transport bits in the TFS, this parameter is used to calculate the rate matching parameter max Nijtti for fixed positions of TrCHs. For more information, refer to 4.2.7.2.1.1 in TS 25.212.

For DPCH, take the following TFS for example, the Block Number of Max TF shall be set to 1, the Block Size of Max TF shall be set to 81.

TFS TF0 0x0
TF1 1x39
TF2 1x81

For S-CCPCH, take the following TFS for example, the Block Number of Max TF shall be set to 3. The same Block Size is applied to multiple blocks in the TFS of S-CCPCH.

TFS TF0 0x168
TF1 1x168
TF2 2x168
TF3 3x168

Flexible Transport Position

This sets the block number of the TF, which has the maximum sigma (RMi*Nij) in the TFCS and it is used to calculate RFi (see 4.2.7.2.2.1 in TS 25.212).

The following example shows the TFS for two transport channels mapped to an S-CCPCH:

TFS of TrCH1 TF0 0x168
TF1 1x168
TF2 2x168
TF3 3x168
TFS of TrCH2 TF0 0x360
TF1 1x360

From the above table, the TFCS would be as follows:

From the above list, using the TFC (TF1, TF1) with the formula shown in TS 25.212, 4.2.7.2.2.1, the value for the Block Number of Max TF setting for each transport channel is 1.

But if the TFCS were to change to allow the following combinations:

TFC (TF3, TF1) when used in the same formula, would make the value of the Block Number of Max TF setting 3 and 1.

It is similar for the DPCH, but with the addition of the Block Size of Max TF parameter, which sets the TF block size. This is required to fulfill the values for the formula from TS 25.212, 4.2.7.2.2.1.

Block Size

Range: 1 to 5000

Default: 244

For the HS-PDSCH, this cell only displays the block size of HS-DSCH. The block size depends on the block size information (Block Size Info) carried in the HS-SCCH and the modulation setting of the HS-PDSCH. The displayed block size is only valid for an HSDSCH Data selection.

The HS-SCCH uses the Block Size values in its coding even when the HS-DSCH is not the HS-PDSCH data type.

Block Size Info

Range: 0 to 63

Default: 0

Sets the block size of HS-DSCH and the Block Size Info coded in HS-SCCH.

For the HS-SCCH channel, the value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable when the Base Channel Configuration is ‘RMC Only’ with STD as the data selection.

When the Base Channel Configuration is of type 'RMC+HSET', the fixed value is still used in the coding of the HS-SCCH.

Block Size of Max TF

Range: 1 to 5000

The behavior of this parameter is dependent upon the Transport Position selection and it is used in combination with the Block Number of Max TF parameter.

Fixed Transport Position

Sets the block size of the TF which has the maximum transport bits in the TFS.

This parameter is just used to calculated the rate matching parameter max Nijtti for fixed positions of TrCHs. For more information, refer to section 4.2.7.2.1.1 in TS 25.212.

For DPCH, take the following TFS for example, the Block Size of Max TF shall be set to 81, the Block Number of Max TF shall be set to 1.

TFS TF0 0x0
TF1 1x39
TF2 1x81

Flexible Transport Position

This sets the block size of the TF, which has the maximum sigma (RMi*Nij) in the TFCS and it is used to calculate RFi (see 4.2.7.2.2.1 in TS 25.212).

Block Size Reference

Range: 0 to 3

Default: 0

Sets the block size reference coded in HS-SCCH Type 2. For more information, refer to section 4.6A.2.2.1.1 in TS25.212.

Block Size Table Type

Range: Bit_Aligned | Octet_Aligned

Default: Bit_Aligned

Sets the transport block size table of HS-DSCH.

This parameter is coupled with Modulation. When Modulation is 64QAM, this parameter is set to Octet_Aligned. When Modulation is 16QAM or QPSK, this parameter can be Octet_Aligned or Bit_Aligned.

Channel Number

View the channel number of the displayed parameters. The software accepts a maximum of 512 channels. You can change the channel configuration or add individual channels using the buttons at the top of the data summary table.

CRC Method

This is a read only setting. The software displays and sets this parameter to Method 2 when the HS-SCCH Type is set to 2 (HS-SCCH less mode). When it is not displayed (HS-SCCH Type 1 or 3 selection), the software uses CRC Method 1.

This parameter is available with only the Adv W-CDMA/HSPA+ DL Rel 10 carrier.

Data

ClosedChoices and Default values vary by channel type.

Channel Type

Choices/Default Values

Notes

CPICH

The data for this channel has a fixed 8-bit binary value of 00000000.

 

DCH, DPCH, E-AGCH, OCNS

Choices: PN9 | PN15 | User Defined Bits

Default: PN9

 

S-CCPCH

Choices: PN9 | PN15 | User Defined Bits | FACH/PCH

Default: PN9

When FACH/PCH is selected, user can set the number of transport channels by setting the Number of FACH/PCH.

E-HICH, E-RGCH

Choices: 0 to 39

Default: 0

This value determines the signature hopping pattern, which is described in TS 25.211.

HS-PDSCH

Choices: PN9 | PN15 | User Defined Bits | HS-DSCH

Default: PN9

Value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable in when the Base Channel Configuration is ‘RMC Only'.

HS-SCCH

Choices: PN9 | PN15 | User Defined Bits | STD

Default: STD

Value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable in when the Base Channel Configuration is ‘RMC Only’.

P-CCPCH

Choices: PN9 | PN15 | User Defined Bits | BCH

Default: BCH

 

PICH

Choices: PN9 | Paging Indicator | User Defined Bits

Default: Paging Indicator

 

When you click the cell, a dialog box button ( ) appears and provides access to Data Source Selection dialog box where you select the data type.

Data Reset at Frame Start

Choices: True | False

Default: True

Sets whether to reset the continuous data at the frame start.

Data Reset at Frame Start is editable only when data is PN or User Defined Bits.

DTX

Choices: Dummy | True

Default: Dummy

Double-click or use the drop-down menu to select the DTX in HS-PDSCH and HS-SCCH.

E-RNTI

Range: 0, 1, 2, ..., 65535

Default: 0

For the E-AGCH channel, this cell sets the E-RNTI. The E-RNTI is the E-DCH Radio Network Identifier defined in TS 25.331. For more information, refer to section 4.10.2 in TS 25.212.

HARQ Acknowledgment Indicator

Range: -1, 0, 1

Default: 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0

Sets the HARQ Acknowledgment Indicator pattern. The format of the input value of HARQ Acknowledgement Indicator is the same as that of Absolute Grant Scope in E-AGCH.

HARQ: ACK/NACK Pattern

Choices: ACK ALL | NACK ALL

Default: ACK ALL

For the HS-SCCH and HS-PDSCH channels, Double-click or use the drop-down menu to select the ACK/NACK pattern of the HS-DSCH.

To view this parameter on the HS-PDSCH or the HS-SCCH, the data selection must be HSDSCH for the HS-PDSCH and STD for the HS-SCCH. For both channels with the correct data selection, this parameter is active and used by the software only with the ARQ Type cell set to HARQ.

HARQ: Maximum Number of HARQ Transmission

Range: 1 to 8

Default: 4

For the HS-SCCH and HS-PDSCH channels, sets the maximum number of HARQ transmission.

To view this parameter on the HS-PDSCH or the HS-SCCH, the data selection must be HSDSCH for the HS-PDSCH and STD for the HS-SCCH. For both channels with the correct data selection, this parameter is active and used by the software only with the ARQ Type cell set to HARQ.

HARQ: Redundancy Version Parameter Sequence

Range: [0 to 7],[0 to 7],[0 to 7],[0 to 7],[0 to 7],[0 to 7],[0 to 7],[0 to 7]

Default: 0,0,0,0

For the HS-SCCH and HS-PDSCH channels, sets the sequence of RV parameters for HARQ feedback control.

To view this parameter on the HS-PDSCH or the HS-SCCH, the data selection must be HSDSCH for the HS-PDSCH and STD for the HS-SCCH. For both channels with the correct data selection, this parameter is active and used by the software only with the ARQ Type cell set to HARQ.

 

HS-DSCH Data

Choices: PN9 | PN15 | User Defined Bits

Default: PN9

This cell is available only when HSDSCH is the current data selection for the HS-PDSCH.

For the HS-PDSCH channel type, when you click the cell, a dialog box button ( ) appears and provides access to Data Source Selection dialog box where you select the data type.

HS-DSCH Incremental Redundancy Buffer Size

Range: 960 to 2073600

Default: 9600

Sets the IR Buffer size per HARQ process of the HS-DSCH in the HS-PDSCH.

This value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable when the Base Channel Configuration is ‘RMC Only’ with an HS-PDSCH data selection of HSDSCH.

HS-PDSCH Code Offset

Range: 1 to 15

Default: 1

Sets the code offset of the HS-PDSCH, coded in the HS-SCCH and active with the STD data selection.

HS-PDSCH Modulation

Choice: QPSK | 16QAM | 64 QAM

Default: 16QAM

Double-click or use the drop-down menu to select the modulation-type for HS-PDSCH that is coded in the HS-SCCH.

This parameter is coupled with the Block Size Table Type parameter on the HS-PDSCH.

The value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable in HS-SCCH when the Base Channel Configuration is ‘RMC Only’ with the STD data selection.

When Modulation is set to 64QAM for HS-PDSCH, the parameter should follow this formula: |O - 1 – (P/8) * 15| mod 2 = (HS-SCCH number) mod 2. Where P is HS-PDSCH Number of Codes, O is HS-PDSCH Code Offset.

If it is not fulfilled, an error message is shown on status bar, the message can also be find in Tools->Status Window. You need modify the HS-PDSCH Code Offset to fulfill the formula.

HS-PDSCH Number of Codes

Range: 1 to 15

Default: 2

Sets the number of codes of the HS-PDSCH, coded in HS-SCCH.

The value is editable when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and when the Base Channel Configuration is of type ‘RMC Only’ the value is fixed and coupled to HS-PDSCH.

HS-SCCH Order

Range: Pattern with 0 and 1 | 000-111

Default: 000

Sets HS-SCCH order coded in HS-SCCH 'type 1' or 'type 3'. It is grayed out when HS-SCCH type is 'type 2'. See 3GPP 4.6C in TS25.212.

HS-SCCH Order State

Range: On | OFF

Default: OFF

Double-click or use the drop-down menu to turn the HS-SCCH order on or off.

This parameter is coupled with HS-SCCH Type, when HS-SCCH Type value is set to Type 2, HS-SCCH Order State is set to Off and grayed out.

HS-SCCH Order Type

Range: Pattern with 0 and 1 | 000-111

Default: 000

Sets HS-SCCH order type coded in HS-SCCH 'type 1' or 'type 3'. It is grayed out when HS-SCCH type is 'type 2'. See 3GPP 4.6C in TS25.212.

HS-SCCH Type

Range: Type 1 | Type 2 | Type 3

Default: Type 1

Double-click or use the drop-down menu to select HS-SCCH type:

● Type1 − The normal HS-SSCH Type .

● Type2 − HS-SSCH Less Operation.

● Type3 − the UE is configured in MIMO mode.

For the HS-PDSCH, this parameter is available only with the Adv W-CDMA/HSPA+ DL Rel 10 carrier.

Inter TTI

Range:1 to 16

Default: 1

For HS-PDSCH and HS-SCCH, this cell sets the inter transmission time interval. This parameter is coupled between the HS-PDSCH and the HS-SCCH. When changed on one channel, it changes on the other channel.

The value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable when the Base Channel Configuration is ‘RMC Only’ with the correct channel data selection of STD for the HS-SCCH and HSDSCH for the HS-PDSCH.

LAC

Range: [0 to F][0 to F][0 to F][0 to F]

Default: 0080

Location Area Code (2 Octets). LAC is used when P-CCPCH Data is BCH and BCH Data is BCCH-BCH-Message.

When BCH Data is not set to BCCH-BCH-Message, the software ignores this value.

MCC

Range: [0 to 9][0 to 9][0 to 9]

Default: 001

Mobile Country Code (MCC) is used when PCCPCH Data is set to BCH and BCH Data is set to BCCH-BCH-Message.

When BCH Data is not set to BCCH-BCH-Message, the software ignores this value.

MIMO Mode

Range: None | Single Stream | Dual stream

Default: None

Double-click or use the drop-down menu to select a MIMO precoding mode.

● None − None MIMO Mode. HS-DPCCH will use TxDiversity if “Total Number of Antennas” is 2.

● SingleStream − 1 precoding stream (1 HSDSCH block )mode.

● DualStream − 2 precoding stream(2 HSDSCH block) mode.

When MIMO Mode is set to Dual Stream, the parameter table shows ClosedHS-DSCH2 Settings which is the same as parameters in HS-DSCH1 Settings.

MNC

Range: [0 to 9][0 to 9]

Default: 01

Mobile Network Code (MNC) is used when PCCPCH Data is set to BCH and BCH Data is set to BCCH-BCH-Message.

When BCH Data is not set to BCCH-BCH-Message, the software ignores this value.

Modulation

Choice:

Default:

Double-click or use the drop-down menu to select the modulation type. For the HS-PDSCH this setting is coupled with the HS-PDSCH Modulation parameter on the HS-SCCH.

For HS-PDSCH, the value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable when the Base Channel Configuration is ‘RMC Only’.

Name

View the selected channel type.

Noff1

Default: 2

This cell provides the number of Tx OFF 1 bits within the F-DPCH slot. It is not editable. See 5.3.2.6 in TS 25.211.

Noff2

Default: 16

This cell provides the number of Tx OFF 2 bits within the F-DPCH slot. It is not editable. See 5.3.2.6 in TS 25.211.

Ntpc

Default: 2

This cell provides the number of TPC bits within the F-DPCH slot. It is not editable. See 5.3.2.6 in TS 25.211.

The parameters Noff1, Noff2, and Ntpc are always read-only (not editable). The parameter values are determined by Slot Format. The coupling rules are defined in ClosedTable 16C in TS25.211.

Slot Format #iChannel Bit Rate (kbps)Channel Symbol Rate (kbps)SFBits/Slot

Noff1

Bits/Slot

Ntpc

Bits/Slot

Noff2

Bits/Slot

031.5256202216
131.5256204214
231.5256206212
331.5256208210
431.5256201028
531.5256201226
631.5256201424
731.5256201622
831.5256201820
931.5256200218

Number Code Blocks

Range: 1 to 15

Sets the number of codes blocks for HS-PDSCH or HS-SCCH.

For HS-SCCH, this value is not editable and determined by Block Size Info.

For HS-PDSCH, this value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable when the Base Channel Configuration is ‘RMC Only’ with the HSDSCH data selection.

Number of DCH

Range: 0 to 8

Default: 2

Set the number of DCH in the DPCH. This parameter is available only when DCH is the DPCH data selection.

Number of FACH/PCH

Range: 0 to 8

Default: 2

Set the number of FACH or PCH in the S-CCPCH. This parameter is available only when FACH/PCH is the S-CCPCH data selection.

The number of transport channels is coupled with the Number of FACH/PCH.

Number of Hybrid ARQ Process

Range: 1 to 8

Default: 2

Sets the number of HARQ processes of the HS-SCCH and the HS-PDSCH. The values are coupled between the two channels, so if it is changed on one channel, the change also shows on the other channel.

For the HS-SCCH and HS-PDSCH, this value is fixed (not editable) when the ClosedBase Channel Configuration is of type ‘RMC+HSET’ and editable when the Base Channel Configuration is ‘RMC Only’.

PCI

Range: 0 | 1 | 2 | 3

Default: 0

Enter a value to set the Precoding weight Control Information (PCI).

Pilot Bits

Choices: 0, 8 @ 15 ksps | 0, 8 @ 30 ksps | 0, 8 @ 60 ksps | 0, 8 @ 120 ksps | 0, 16 @ 240 ksps | 0, 16 @ 480 ksps | 0, 16 @ 960 ksps

Set the pilot bits. The number of bits available depends on the data format of the S-CCPCH channel.

Power

Range: -60 to 0 dB

Enter the channel power level relative to the carrier power.

Rate

Choices: see Spreading Code for limits

Double-click or use the drop-down menu to set the channel symbol rate.

For channels that have adjustable symbol rates, you may enter a symbol rate that exceeds the acceptable range, based on the selected spreading code. This condition generates an error, which you correct by selecting a proper spreading code for the symbol rate. The software allows this behavior so that you can set either value first.

Redundancy Version Parameter

Range: 0 to 7

Default: 0

Set the RV (Redundancy Version) parameter of the HS-DSCH, coded in the HS-SCCH. Set this value in either the HS-PDSCH or HS-SCCH.

This parameter is ignored when the ARQ Type parameter is set to HARQ, and is editable when set to NONE and the data type is STD on the HS-SCCH or HSDSCH on the HS-PDSCH.

Relative Grant Value

Range: -1, 0, 1

Default: 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0

For the E-RGCH channel, this cell sets the Relative Grant Value pattern. The format of the input value of relative grant value is the same as that of Absolute Grant Scope in E-AGCH.

Scrambling Code

Range: 0−511

Default: 0

Enter a value to set the channel’s primary scramble code.

This parameter applies to all channels but the PSCH. 

Scramble Offset

Range: 0 to 15

Default: 0

Enter a scramble code offset value. The offset value is multiplied by 16 and added to the scramble code.

This parameter applies to all channels but the PSCH. 

Scramble Type

Choices: STD | LEFT | RIGHT

Default: STD

Double-click or use the drop-down menu to select a scramble type.

This parameter applies to all channels but the PSCH. 

SFN Increment

Choices: On | Off

Default: On

Double-click or use the drop-down menu to turn the SFN on or off in the P-CCPCH channel.

Editable when SFN State cell parameter is set to On. The value is ignored when SFN State is set to Off.

SFN Initial Value

Range: 0 to 4095

Default: 0

Enter the initial value for SFN.

Editable when SFN State cell parameter is set to On. The value is ignored when SFN State is set to Off.

SFN State

Double-click or use the drop-down menu to turn the SFN on or off.

Editable when BCH Data cell parameter is set to PN9, PN15, or User Defined Data. The value is ignored when BCH Data is set to BCCH-BCH-Message.

Signature Sequence Index

Range: 0 to 39

Default: 0

Sets the signature sequence index value. The E-RGCH signature sequence index value in ClosedTable 16B is given by higher layers. For more information, refer to section 5.3.2.4 in TS 25.211.

Slot Format

To enter a value, highlight the existing value and enter the new slot number. The slot format determines rate and spreading code in addition to other control bits.

Channel Type

Range

Default

DPCH

0 to 16

0

F-DPCH

0 to 9

0

Spreading Code

Sets the Closedchannel spread code number which affects the Rate cell limits. The spread code is an OVSF code. Ensure that the value entered does not create a code domain conflict with the other physical channels.

Channel Type

Range

CPICH, E-AGCH,

P-CCPCH, PICH

0-255 @ 15 ksps (fixed rate)

DPCH, OCNS, F-DPCH

0–511 @ 7.5 ksps

0–255 @ 15 ksps

0–127 @ 30 ksps

0–63 @ 60 ksps

0–31 @ 120 ksps

0–15 @ 240 ksps

0–7 @ 480 ksps

0–3 @ 960 ksps

E-HICH, E-RGCH,

HS-SCCH

Range: 0-127 @ 30 ksps

(fixed rate)

HS-PDSCH

Range: 0-15 @ 240 ksps

(fixed rate)

S-CCPCH

0-255 @ 15 ksps

0-127 @ 30 ksps

0-63 @ 60 ksps

0-31 @ 120 ksps

0-15 @ 240 ksps

0-7 @ 480 ksps

0-3 @ 960 ksps

You may enter a spreading code value that exceeds the acceptable range, based on the selected symbol rate. This condition generates an error, which you correct by selecting the proper symbol rate for the spreading code. The software allows this behavior so that you can set either value first.

This parameter, does not apply to the PSCH channel.

E-RGCH and E-HICH

These two channel can use the same spreading code. When both are set to the same spreading code, the software will show this as a conflict by displaying the action to take in Status Bar and Status Window. Resolve the conflict by changing either the Timing Offset or Signature Sequence Index for one of the channels.

State

Double-click or use the drop-down menu to turn the channel on or off.

TFCI

Range: 0 to 1023

Default: 0

In the DPCH and S-CCPCH channels, this cell is the number of TFCI bits sent to each timeslot and is determined by the slot format. The TFCI is an optional field describing what services are in use (for example, data and video). Fixed rate service does not include TFCI.

If this cell is not editable, you can enable it by turning on TFCI Field at the carrier property pane.

TFCI Field

Double-click or use the pull-down menu to turn the TFCI capability on or off.

Turn this cell on to transmit the TFCI bit pattern defined in Channel Setup. It is determined by Slot Format. The coupling rule is defined in ClosedTable 11 in TS 25.211.

TFCI Power

Range: −20 to 20 dB

For the DPCH channel, this cell sets the power level for the TFCI bits.

Timing Offset

E-RGCH and E-HICH—Advanced DL Release 10 Carrier

Choices: 17920 | -10240 | -2560 | 5120 | 12800 | 20480 | 28160 | 35840 | 43520 | 51200

Default: -17920

Select the timing offset for these channels. The value is expressed in chips.

All Other Channels

Range: 0 to 149

Enter a value to set a timing offset for the selected channel. Each integer value entered is equivalent to 256 chips or 1/10 of a timeslot offset.

The timing offset affects the crest factor of the signal. By varying the timing offset, the probability of channels adding in phase and producing a high peak-to-average ratio or crest factor is minimized. Base stations vary the timing between channels so that amplifiers can operate at the most efficient level.

TPC

Range: 0000 to 7FFF

Enter the TPC value for the OCNS channel.

TPC Number of Steps

Range: 1 to 80

Default: 1

For the DPCH channel and the F-DPCH channel, this cell sets the number of up and down power steps for the TPC Pattern selections Up/Down and Down/Up. For example with this cell set to 20 and the TPC Pattern set to Up/Down, the signal source transmits a power pattern that tells the basestation to step-up the power up in 1 dB increments for 20-steps and then down for 20-steps. The signal repeats this pattern until the parameter changes or the signal terminates.

TPC Pattern

Choices: Up/Down | Down/Up | All Up | All Down | User Defined Bits

Default: Up/Down

For the DPCH channel and the F-DPCH channel, this cell sets the TPC (transmit power control) pattern. This pattern instructs the base station to increase or decrease its power in 1 dB increments. When you click the cell, a dialog box button () appears and provides access to the TPC Selection dialog box where you can select from the following choices:

Up/Down

This choice repetitively steps up and down the TPC pattern. Use the TPC Number of Steps cell to set the number of times that the power increases and then decreases.

Down/Up

This choice repetitively steps down and up the TPC pattern. Use the TPC Number of Steps cell to set the number of times that the power decreases and then increases.

All Up

This choice consecutively steps up the TPC pattern.

All Down

This choice consecutively steps down the TPC pattern.

User Defined Bits

This choice activates the User Defined Bits data editor, enabling you to create a custom TPC pattern: 1-power steps up, 0 to 16

Transport Position

Adv W-CDMA/HSPA+ DL Rel 10 Carrier

Choices: Fixed | Flexible

Default: Fixed

Set the transport position type to determine how rate matching is calculated. For more information, see 3GPP TS 25.212.

For the S-CCPCH, this parameter appears with the FACH/PCH Data selection

The choices for this parameter appear in the software's GUI only when Minor Enhancement Update (MEU) Option U01 or greater is valid. Refer to Licenses for more information.

All other Carriers

This is a fixed position only (not editable).

TTI

Choices: 10 ms | 20 ms | 40 ms | 80 ms

Default: 40 ms

For the HS-PDSCH and HS-SCCH channels, this value is fixed (not editable).

For the S-CCPCH Transport Channels, you can select the FACH or PCH TTI.

UE ID

Range: 0 to 65535

Default: 0

For the HS-SCCH channel, this sets the identity of UE under test.

Dedicated Transport Channel

The DCH settings are available only after selecting DCH as the DPCH Data type. To add or remove DCHs, use the Number of DCH cell.

Data

Choices: PN9 | PN15 | User Defined Bits

Default: PN9

When you click the cell, a dialog box button ( ) appears and provides access to Data Source Selection dialog box where you select the data type. This cell is available only when DCH is the DPCH data selection, or, when FACH or PCH is the S-CCPCH data selection.

Block Size

Range: 1 to 50000

Default: 244

Sets the coupling block size for the selected dedicated transport channel DCH/FACH/PCH. This cell is available only when DCH is the DPCH data selection, or, when FACH or PCH is the S-CCPCH data selection.

Coding Type

Choices: 1/2 rate convolutional encoder | 1/3 rate convolutional encoder | turbo coder | no coding

Default: 1/3 rate convolutional encoder

Double-click or use the drop-down menu to set the DCH/FACH/PCH coding type. This cell is available only when DCH is the DPCH data selection, or, when FACH or PCH is the S-CCPCH data selection.

CRC

Choices: 0 | 8 | 12 | 16 | 24

Default: 16

Double-click or use the drop-down menu to set the DCH/FACH/PCH cyclic redundancy bits. This cell is available only when DCH is the DPCH data selection, or, when FACH or PCH is the S-CCPCH data selection.

Number of Blocks

Range: 1 to 512

Default: 1

Sets the DCH/FACH/PCH Number of Blocks. This cell is available when DCH is the DPCH data selection, or, when FACH or PCH is the S-CCPCH data selection.

Rate Matching Attribute

Range: 1 to 256

Default: 256

On the DPCH, enter a DCH rate matching attribute. This cell is available only when DCH is the DPCH data selection.

On the S-CCPCH, enter a FACH or PCH rate matching attribute. This cell is available only when FACH/PCH is the S-CCPCH data selection.

TTI

Choices: 10 ms | 20 ms | 40 ms | 80 ms

Default: 40 ms

Double click or use the pull-down menu to set the TTI for the selected channel. This cell is available only when DCH is the DPCH data selection.

S-CCPCH Transport Channel

The Transport Channel settings are available only after selecting FACH/PCH as the S-CCPCH Data type. To add or remove FACH/PCH, use the Number of FACH/PCH cell.

TFCI Field, TFCI, Pilot Bits are determined by Slot Format. The coupling rule is defined in Table 18 in TS 25.211.

When the Ntfci in Table18 (TS 25.211) is 0, TFCI is grayed out and TFCI Field is set to Off. When the Ntfci is not 0, TFCI is valid to set and TFCI Field is set to On.

When the Slot Format value is less than 8, the TFCI Field is read only. When the Slot Format value is more than 7, the TFCI Field is valid to set, if it is turn off, DTX shall be used in TFCI field. Only the S-CCPCH with QPSK is supported.

If the puncture rate of a transport channel with turbo coding exceeds 2/3, an error message is shown on the status bar.

Configuring the Channel Setup View

Data Selection Dialog Box

Downlink Channel Structure

Frame Structures

Marker Selection Dialog Box

Understanding TFCI, TPC and Pilot Power Offsets

Understanding TPC Values

User Interface Basics