Real Time

2. Basic

The following figure is a composite of all supported instruments, so some parameters may not apply to your instrument.

2. Basic: Relative Amplitude (PXB)

2. Basic: Baseband Channel Assignment (PXB)

2. Basic: RF Output Port (EXT)

Frequency

Range: for specified range values, see the signal generator's data sheet

Enter a value to set the signal generator’s output frequency. Use abbreviations for faster entry (example: 1g = 1.000000000000 GHz).

Amplitude

ESG, PSG, EXT, EXG, or MXG

Range: for amplitude range values, see the signal generator's data sheet

Enter a value to set the signal generator’s output amplitude in dBm.

Relative Amplitude (PXB)

PXB Baseband Generator and Channel Emulator

In a typical MIMO system, the average power of the signal transmitted by each antenna is different than the average power transmitted by the other antennas. For example, a difference in average power can be caused by preambles or other reference signals that are present on some antennas and not on others.

When connected to a PXB Baseband Generator and Channel Emulator, Signal Studio provides a separate Relative Amplitude cell for each antenna to display this difference in average power. For example, if you set up a two-antenna configuration in the System Configuration Wizard, the software displays two Relative Amplitude cells.

When you generate the waveform, the software sets the power in the Relative Amplitude cells based on the current waveform settings. The value in each Relative Amplitude cell represents the power in the corresponding baseband generator (BBG) on the PXB relative to the power in the other BBGs.

For more information, refer to the PXB's online documentation.

Baseband Channel Assignment (PXB)

Range: 1 to 16

Default: 1

When you establish a connection between the Signal Studio software and the PXB, Signal Studio recognizes the number of baseband generators (BBGs) in the currently loaded PXB configuration. Signal Studio creates a waveform file (Ant0, Ant1, Ant2, and so on) for each antenna configured in the System Configuration Wizard. The default behavior is for Signal Studio to download waveform file Ant0 to BBG1 in the PXB, waveform file Ant1 to BBG2, and so on. In the Baseband Channel Assignment cell, the default BBG assignments are displayed as a comma-separated list (1,2).  

The Baseband Channel Assignment parameter enables you control the assignment of each waveform file to a specific BBG resource, rather than accepting the default. You can assign Ant0 to BBG2 and Ant1 to BBG1 by making the corresponding change to the comma separated list (2,1).

RF Output

Double-click or use the drop-down menu to control the signal generator’s RF output state.

RF Output Port (EXT)

Choice: RF Out | RFIO 1 | RFIO 2

Default: RF Out

Double-click or use the drop-down menu to select the signal generator’s RF output port. This parameter is only available when connected to the E6607 EXT.

Hardware

Waveform Setup