|
|
This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. |
|
|
This button displays in place of the Setting Current button. It indicates that the instrument settings are not current and need to be updated with the new software settings. Click this button to update the instrument's settings. |
Range: 2560 to 51200 ms, Step: 2560 ms
Default: 2560 ms
Sets the segment length (Group 1 + Group 2). The segment length is clipped by a multiple number of the CFN cycle length (2560 ms).
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:CFACh:SEGMent:LENGth
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:CFACh:SEGMent:LENGth?
Indicates the segment length in the SFN cycle (2560 ms).
Indicates the Segment information. (Timing, Length)
Indicates the start position of Group 1. This value is fixed to 0. This value does not include the system synchronization trigger delay.
Indicates the length of Preamble part in Group 1.
Shows the start position of DPCCH only part in Group 1. This value does not include the system synchronization trigger delay.
Indicates the length of DPCCH only part in Group 1.
Indicates the length of E-DCH part in Group 1.
Indicates the length of DTX part in Group 1.]
Shows the start position of Group 2, distance from Group 1 Start Position. The start position of Group2 fits the boundary of 10 ms frame. This value does not include the system synchronization trigger delay.
Indicates the length of E-DCH part in Group 2.
Shows the length of DTX part in Group 2.