|
|
This button indicates that the current real-time settings have been applied to the instrument—no action is required. This button is not available when the Apply Needed button is active. |
|
|
This button displays in place of the Setting Current button. It indicates that the instrument settings are not current and need to be updated with the new software settings. Click this button to update the instrument's settings. |
|
|
This button opens the RMC/FRC Wizard dialog box. This dialog box can be used to set up the Reference Measurement Channel (RMC) or the Fixed Reference Channel (FRC). |
|
|
This tab accesses the 1. General Settings parameters. |
|
|
This tab accesses the Code Domain Graphics dialog box. |
Range: 0 to 16777215
Default: 0
Sets the scrambling code number.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:SCRamblecode <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:SCRamblecode?
Controls the states and power levels for the uplink channels. Also, displays the channel coding, spreading factor (SF), and data-type information.