In the uplink, the Enhanced Dedicated Physical Data Channel (E-DPDCH) is the physical channel used by the Enhanced Dedicate Control Channel (E-DCCH) to transmit user data.
|
1. E-DPDCH |
2. E-DCH |
|---|---|
|
Miscellaneous Information (E-DCH) |
|
|
|
|
|
|
|
|
Miscellaneous Information (E-DPDCH) |
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
This section defines the Settings Current and Apply Needed buttons. Only one button is available at any time. These buttons are available in all of the W-CDMA/HSPA+ Uplink's tree nodes.
|
|
This button indicates that the current real-time settings have been applied to the instrument. No action is required. |
|
|
This button indicates that the instrument settings are not current and need to be updated to be applied to the instrument. Click this button to update the instrument's settings. [:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:APPLy [:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:APPLy? |
Choice: Off | On
Default: On
Enables or disables the E-DPDCH state.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch[:STATe] ON|OFF|1|0
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch[:STATe]?
Range: –40 to 0 dB
Default: 0 dB
Set the E-DPDCH power in dB. This power is assigned to each E-DPDCH when multiple E-DPDCHs are configured. The entered power is typically set to the channels as SF4. Where the E-DPDCHs are configured to SF2x2 + SF4x2, the channel power of SF2 is 3.01 dB higher than the entered power.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:POWer <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:POWer?
Range: –40 to 0
Default: 0
Set the power of the alternate E-DPDCH setting in dB. This field is disabled when TFC E-TFCI Pattern is MAIN ALL. This power is assigned to each e_DPDCH when multiple E-DPDCHs are configured. The entered power is set to the channels as SF4. Where the E-DPDCHs are configured to SF2x2 + SF4x2, the channel power of SF2 is 3.01 dB higher than the entered power.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:POWer <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:POWer?
Choice: SF256x1 | SF128x1 | SF64x1 | SF32x1 | SF16x1 | SF8x1 | SF4x1 | SF4x2 | SF2x2 | SF2x2+SF4x2 | AUTO
Default: SF4x1
Select Spreading Factor (SF) and Number of E-DPDCHs configuration on the main setting.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:SNPHchs SF256|SF128|SF64|SF32|SF16|SF8|SF4|SF4SF4|SF2SF2|SF4SF4SF2SF2|AUTO
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:SNPHchs?
Choice: SF256x1 | SF128x1 | SF64x1 | SF32x1 | SF16x1 | SF8x1 | SF4x1 | SF4x2 | SF2x2 | SF2x2+SF4x2
Default: SF4x1
Select Spreading Factor (SF) and Number of E-DPDCHs configuration on the alternate setting. This field is disabled when TFC E-TFCI Pattern is MAIN ALL.
|
SF256x1 |
Set the spreading factor to 256 and the number of E-DPDCH to 1 |
|
SF128x1 |
Set the spreading factor to 128 and the number of E-DPDCH to 1 |
|
SF64x1 |
Set the spreading factor to 64 and the number of E-DPDCH to 1 |
|
SF32x1 |
Set the spreading factor to 32 and the number of E-DPDCH to 1 |
|
SF16x1 |
Set the spreading factor to 16 and the number of E-DPDCH to 1 |
|
SF8x1 |
Set the spreading factor to 8 and the number of E-DPDCH to 1 |
|
SF4x1 |
Set the spreading factor to 4 and the number of E-DPDCH to 1 |
|
SF4x2 |
Set the spreading factor to 4 and the number of E-DPDCH to 2 |
|
SF2x2 |
Set the spreading factor to 2 and the number of E-DPDCH to 2 |
|
SF2x2+SF4x2 |
Set the spreading factor to 4 for 2 E-DPDCHs and the spreading factor to 2 for 2 E-DPDCHs |
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:SNPHchs SF256|SF128|SF64|SF32|SF16|SF8|SF4|SF4SF4|SF2SF2|SF4SF4SF2SF2
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]EDPDch:SNPHchs?
Choice: SF256x1 | SF128x1 | SF64x1 | SF32x1 | SF16x1 | SF8x1 | SF4x1 | SF4x2 | SF2x2 | SF2x2 + SF4x2
Default: SF2x2 + SF4x2
Select Spreading Factor (SF) and the number of E-DPDCHs configuration. This field is enabled when SF and Number of E-DPDCHs is "AUTO".
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:MCCodes SF256|SF128|SF64|SF32|SF16|SF8|SF4|SF4SF4|SF2SF2|SF4SF4SF2SF2
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:MCCodes?
Choice: QPSK (2 x BPSK) | 16QAM (2 x 4PAM)
Default: QPSK
Set the E-DPDCH modulation capability
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:MCAPability QPSK|QAM16
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:MCAPability?
Range: 0.44 to 1.0
Default: 0.44
Set the PL non-max E-DPDCH setting. This field is enabled when SF and Number of E-DPDCHs is AUTO.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:PLNMax <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:PLNMax?
Choice: PN9 | FIX4 | E-DCH | Custom Pattern| User File
Default: E-DCH
Edit the Data of the uplink E-DPDCH by clicking on the cell. Then click on the dialog box icon
to launch the
Data dialog box. When E-DCH is selected, this applies the defined data in the E-DCH data and to the E-DCH coding.
When loading a user file through the software's Data dialog box, the MXG/EXG requires an ASCII text file consisting of 1s and 0s. When using SCPI commands, all instruments require a binary data file.
|
E-DCH |
This choice selects the transport channel as the data source. |
|
Custom Pattern |
Sets the E-DPDCH data pattern to Custom Pattern. The value of this command is a string which is represented ‘0’ or ‘1’. The maximum data length is 81,920 patterns. |
|
"<filename>" |
This variable represents a data pattern file stored in instrument memory. The data pattern must contain at least one bit or the Play function will not work . |
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:DATA PN9|FIX4|EDCH|PATTern|"<filename>"
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:DATA?
If you select <"filename">, PATTern or FIX4, use the following commands to create the pattern:
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:DATA:FIX4 <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:DATA:FIX4?
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:DATA:PATTern <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:DATA:PATTern?
Indicates the Binary Channel Bits per TTI (N-BIN). The alternate field is disabled when TFC E-TFCI Pattern is set to MAIN ALL. This parameter is not editable.
Indicates the IQ branch assignment [I or Q] of E-DPDCH. When multiple E-DPDCHs are configured, multiple IQ assignment are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL. This parameter is not editable.
Indicates the E-DPDCH Channel Code that is currently configured. When multiple E-DPDCHs are configured, multiple Channel Code assignments are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL. This parameter is not editable.
Indicates the E-DPDCH Spreading Factor(s) that is currently configured. When multiple E-DPDCHs are configured, multiple Spreading Factor assignments are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL. This parameter is not editable.
Indicates the E-DPDCH Bit Rate [kbps] that is currently configured. When multiple E-DPDCHs are configured, multiple bit rate assignments are indicated. The alternate field is disabled when TFC E-TFCI Pattern is MAIN ALL. This parameter is not editable.
Choice: PN9 | FIX4 | Custom Pattern | User File
Default: PN9
Edit the Data (Main) of the uplink E-DCH by clicking on the cell. Then click on the dialog box icon
to launch the
Data (Main) dialog box.
When loading a user file through the software's Data dialog box, the MXG/EXG requires an ASCII text file consisting of 1s and 0s. When using SCPI commands, all instruments require a binary data file.
|
PN9 |
Sets E-PCH data pattern to PN9. |
|
FIX4 |
Sets the E-DPCCH data pattern to FIX4 (4-bit binary). |
|
Custom Pattern |
Sets the E-DCH data pattern to Custom Pattern. The value of this command is a string which is represented ‘0’ or ‘1’. The maximum data length is 81,920 patterns. |
|
"<filename>" |
This variable represents a data pattern file stored in instrument memory. The data pattern must contain at least one bit or the Play function will not work. |
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:EDCH:DATA PN9|FIX4|PATTern|"<filename>"
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:EDCH:DATA?
If you select <"filename">, PATTern or FIX4, use the following commands to create the pattern:
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:EDCH:DATA:FIX4 <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:EDCH:DATA:FIX4?
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:EDCH:DATA:PATTern <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:EDPDch:EDCH:DATA:PATTern?
Choice: PN9 | FIX4 | Custom Pattern | User File
Default: PN9
Edit the Data (Alternate) of the uplink E-DCH by clicking on the cell. Then click on the dialog box icon
to launch the
Data (Alternate) dialog box. This field is disabled when the TFC E-TFCI Pattern is set to Main All.
|
PATTern |
Sets the data of the alternate E-DCH to Custom Pattern. The value of this command is a string which is represented ‘0’ or ‘1’. The maximum data length is 81,920 patterns. |
|
"<filename>" |
This variable represents a data pattern file stored in instrument memory. The data pattern must contain at least one bit or the Play function will not work. |
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:EDCH:DATA PN9|FIX4|PATTern|"<filename>"
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:EDCH:DATA?
If you select <"filename">, PATTern or FIX4, use the following commands to create the pattern:
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:EDCH:DATA:FIX4 <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:EDCH:DATA:FIX4?
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:EDCH:DATA:PATTern <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:HSUPa:TFC[:ALT]:EDPDch:EDCH:DATA:PATTern?
Indicates the CRC Length of E-DCH. This parameter is not editable.
Indicates the Coding Type of E-DCH. This parameter is not editable.
Indicates the Coding Rate of E-DCH. This parameter is not editable.
Indicate the Puncture Rate [%]. The puncture rate should be greater than 33 %. This parameter is not editable.
Puncture Rate [%] = Ne,data,j / Ne,j * 100. [defined in 3GPP STD TS 25.212 4.8.4.1]