These settings control the real-time baseband and W-CDMA functionality.
For more information, refer to the Multi PRACH Settings tab and to the PRACH Structure tab.
|
1. General Settings |
2. Transmission Settings |
3. Trigger Settings |
|---|---|---|
|
|
|
This section defines the Settings Current and Apply Needed buttons. Only one button is available at any time. These buttons are available in all of the W-CDMA/HSPA+ Uplink's tree nodes.
Choice: Single|Multiple
Default: Single
Sets the PRACH generation type.
|
Single |
This choice generates a single PRACH. |
|
Multiple |
This choice generates up to eight PRACHes. |
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:MODE[:SELect] SINGle|MULTi
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:MODE[:SELect]?
Range: 1 to 2147483647 | Infinity
Default: 1
Sets the repetition number of PRACH (Preamble + Message part).
|
Infinity |
This choice means the repeating number will continue while the PRACH mode is selected and the start trigger is ignored. |
If the parameter set by the following command is changed while the signal is active, the :ULINk:APPLy command or Apply Needed (
) button must be executed for the change to occur.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh[:SINGle]:NUMBer <val>|INFinity
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh[:SINGle]:NUMBer?
Range: 1 to 2147447836 | Infinity
Default: 1
Sets the repetition number of PRACH (80 ms Multiple PRACH configuration).
If the parameter set by the following command is changed while the signal is active, the :ULINk:APPLy command or Apply Needed (
) button must be executed for the change to occur.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:MULTi:NUMBer <val>|INFinity
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:MULTi:NUMBer?
Range: 0 to 11
Default: 0
Sets the sub-channel number for starting of the PRACH signal.
If the parameter set by the following command is changed while the signal is active, the :ULINk:APPLy command or Apply Needed (
) button must be executed for the change to occur.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:SUBChannel <val>
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:SUBChannel?
Choices: Immediate|Trigger
Default: Immediate
Sets the trigger source of PRACH.
Immediate: This choice resets the waveform and immediately replays waveform from the start.
Trigger: This choice plays the waveform after receiving the PRACH start trigger.
If the parameter set by the following command is changed while the signal is active, the :ULINk:APPLy command or Apply Needed (
) button must be executed for the change to occur.
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:TRIGger:SOURce IMMediate|TRIGger
[:SOURce]:RADio:WCDMa:TGPP[:BBG]:ULINk:PRACh:TRIGger:SOURce?