These setting control the CELL_FACH real-time Channel Settings.
This section defines the W-CDMA/HSPA+ CELL_FACH's buttons. With the exception of the RMC/FRC Wizard button, the Restore Default Settings button is available in all of the W-CDMA/HSPA+ Uplink (CELL_FACH) > Channel's tree nodes.
|
Restores all of the W-CDMA/HSPA+ channel's parameters to their default conditions. |
Range: 2560 to 51200 ms, Step: 2560 ms
Default: 2560 ms
Sets the segment length (Group 1 + Group 2). The segment length is clipped by a multiple number of the CFN cycle length (2560 ms).
Indicates the segment length in the SFN cycle (2560 ms).
Indicates the start position of Group 1. This value is fixed to 0. This value does not include the system synchronization trigger delay.
Indicates the length of Preamble part in Group 1.
Shows the start position of DPCCH only part in Group 1. This value does not include the system synchronization trigger delay.
Indicates the length of DPCCH only part in Group 1.
Indicates the length of E-DCH part in Group 1.
Indicates the length of DTX part in Group 1.]
Shows the start position of Group 2, distance from Group 1 Start Position. The start position of Group2 fits the boundary of 10 ms frame. This value does not include the system synchronization trigger delay.
Indicates the length of E-DCH part in Group 2.
Shows the length of DTX part in Group 2.