These setting control the PRACH real-time Channel Settings.
Refer to RMC/FRC Wizard.
|
1. General |
|---|
This section defines the W-CDMA/HSPA+ PRACH's buttons. With the exception of the RMC/FRC Wizard button, these buttons are available in all of the W-CDMA/HSPA+ Uplink (PRACH) > Channel's tree nodes.
|
Restores all of the W-CDMA/HSPA+ channel's parameters to their default conditions. |
|
Begins the PRACH transmission. This button is active when the PRACH Start Trigger Source is set to Trigger in the PRACH node. |
|
Opens the RMC/FRC Wizard window for the channel. |
Range: 0 to 8191
Default: 0
Sets the scrambling code number for the PRACH.