These settings control the real-time transmission gap pattern functionality.
There are 6 TGPS.
The
Compressed Mode Start and
stop buttons are enabled when the State is On, Compressed Mode Trigger Source is set to Trigger, and or one or more TGPSn are active.
Refer to Compressed Mode - General Settings.
|
1. TGPSn |
|---|
Choice: Active | Inactive
Default: Inactive
Sets the state of the gap pattern in the compressed mode setting. The state on the general settings tab should be set to "On" to enable the compressed mode.
Range: 0 to 255
Default: 0
Sets the connection frame number (CFN) of the first radio frame of the first pattern within the transmission gap pattern.
Range: 0 (Infinity) to 511
Default: 0 (Infinity)
Sets the number of transmission gap patterns in the transmission gap pattern sequence. Set TGPRC to 0 for infinite pattern repetition.
Range: 0 to 14 (Slot)
Default: 11 (Slots)
Sets the transmission gap starting slot number (TGSN). TGSN is the slot number of the first transmission gap slot in the first radio frame of the transmission gap pattern
Choice: 3 | 4 | 5 | 7 | 10 | 14 (Slot)
Default: 7 Slots
Sets the TGL1 value, expressed in number of slots.
Choice: Omitted (TGL2 = TGL1) | 3 | 4 | 5 | 7 | 10 | 14 (Slot)
Default: Omitted
Sets the TGL2 value, expressed in number of slots. If the Omitted is selected, TGL2 = TGL1.
Range: 0 (Undefined), 15 to 269 (Slot)
Default: 0 Slot
Sets the transmission gap start distance (TGD), which is the duration between the starting slots of two consecutive transmission gaps within a transmission gap pattern, expressed in number of slots. If TGD = 0, then only one transmission gap is available in the transmission gap pattern.
Range: 1 to 144 (Frame)
Default: 2 Frames
Sets the transmission gap pattern length (TGPL1), expressed in number of frames.
Choice: SF/2 | Higher Layer
Sets the DPCH compression mode method.