These settings control the real-time transmission power control functionality for the W-CDMA/HSPA+ (CELL_FACH) signal.
|
1. General Settings |
|---|
| Initial Power (Group 2) |
| Up/Down Pattern |
This section defines the W-CDMA/HSPA+ CELL_FACH's buttons. With the exception of the RMC/FRC Wizard button, the Restore Default Settings button is available in all of the W-CDMA/HSPA+ Uplink (CELL_FACH) > Channel's tree nodes.
|
Restores all of the W-CDMA/HSPA+ channel's parameters to their default conditions. |
Choice: Off | On
Default: Off
Enables or disables the transmission power control.
Default: 0 dB
Indicates the maximum power in dB for transmission power control limit.
Range: -40 to 0 (dB)
Default: -40 dB
Sets the minimum power in dB. The down power control is ignored when the transmission power has reached this power level.
Choice: 0.5 | 1.0 | 2.0 | 3.0 (dB)
Default: 0.5 dB
Sets the power step of the transmission power control in dB.
Range: -40 to 0 dB
Default: 0 dB
Sets the initial power of Group 1 in dB. The value must be bigger than or equal to the value set for the Minimum Power.
Range: -40 to 0 dB
Default: 0 dB
Sets the initial power of Group 2 in dB. The value must be bigger than or equal to the value set for the Minimum Power.
Choice: Custom Pattern | External
Default: External
Select the transmission power control up/down pattern.
Clicking Custom Pattern opens an
extended Up/Down window (i.e. for setting: Length, Fill Pattern, Start Index, Fill Length, Interval, Value, ...).