These settings control the real-time baseband and W-CDMA/HSPA+ DPCCH/DPDCH functionality.
|
1. General Settings |
|---|
| Channel Configuration Mode |
This section defines the W-CDMA/HSPA+ DPCCH/DPDCH's buttons. The Restore Default Settings button is available in all of the W-CDMA/HSPA+ Uplink (DPCCH/DPDCH) > Channel's tree nodes.
|
Restores all of the W-CDMA/HSPA+ channel's parameters to their default conditions. |
|
Enables you to quickly duplicate settings from one resource to another like resource.. Refer to the N5106A's Toolbar topic. |
|
Enables you to quickly duplicate settings from one resource to another like resource.. Refer to the N5106A's Toolbar topic. |
Choice: DPCCH/DPDCH | PRACH | CELL_FACH
Default: DPCCH/DPDCH
Double-click or use the drop-down menu to set the channel configuration mode.
Choice: Root Nyquist | Nyquist | Gaussian | Rectangle | IS95 | IS95 w/EQ | IS95 Mod | IS95 Mod w/EQ | APCO 25 C4FM | UN3/4 GSM Gaussian | User FIR Filter | User File
Default: Root Nyquist (Alpha = 0.220)