Using the System Configuration Wizard

From the menu bar, click System and select Run System Configuration Wizard from the drop-down menu that appears. A sequence of windows steps you through configuring the hardware for your application and saving the setup for later use.

In each window:

Step 1- Select a hardware configuration.

Choose a supported hardware configuration from the Closeddisplayed list.

Step 2- Select a specific hardware system.

You can either configure a new system or select a previously saved hardware configuration:

Choose <New> to Closedconfigure a new system.

Step 3- Enter the connection information for one of the following:

or

Step 4- The software tests the I/O connection and confirms a Pass or Fail status for the connected hardware. (You can also click the Test I/O button in Step 3 to confirm the connection.)

Step 5- Enter a name of your choice for the system and click Finish to begin using this setup.  

ClosedSelect a previously saved hardware system configuration from the list displayed.

Step 3- The software tests the I/O connection and confirms a Pass or Fail status for the connected hardware.