RACH

The Reverse Access Channel (RACH) is used by the mobile station to initiate communication with the base station and to respond to Paging Channel messages.

1. General

2. Frame

State

Frame Length

Power

Frame Offset

Radio Configuration

EbNo

Data

 

Bit Rate

 

Channel Coding

 

BER Insertion

 

RACH Configuration Summary Table

This section defines the Settings Current and Apply Needed buttons. Only one button is available at any time. These buttons are available in all of the CDMA2000's tree nodes.

This button sets all channels to equal power, and the total power to 0 dB.

This button scales all of the current channel powers so that the total power equals 0 dB, keeping the previous power ratios between the individual channels.

1. General

State

Choice: On | Off

Set operating state of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH[:STATe] ON|OFF|1|0

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH[:STATe]?

Power

Range: -40 to 0 dB

Set the power of the channel in dB.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:POWer <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:POWer?

Radio Configuration

Choice: 1 | 2

Set the Radio Configuration of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:RCONfig 1|2

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:RCONfig?

Data

Choice: PN9 | PN15 | Pattern | UserFile

Default: PN9

Edit the data pattern for the Reverse Fundamental Traffic Channel (RFCH) by clicking on the cell. Then click on the dialog box icon to launch the Closedselection dialog box.

Set the data of the channel. In the User File case, 0,1 txt file or binary file can be selected as the data source

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:DATA PN9|PN15|FIX4|"<file name>"

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:DATA?

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:DATA:FIX4 <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:DATA:FIX4?

Bit Rate (bps)

Display the bit rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:RATE?

Channel Coding

Choice: All On | All Off

Set the channel code state of the channel.

If the coding state is off, the channel will be no channel coding and interleaver.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH: CCODing 0|1|ON|OFF

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH: CCODing ?

BER Insertion

Range: 0.00% to 50%

Set the bit error rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:BER <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:BER?

2.Frame

Frame Length (ms)

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:FLENgth?

Frame Offset (ms)

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:FOFFset <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:FOFFset?

EbNo

Range:

Min: -30 + 10log10(ChipRate/BitRate) + NormalizedPower dB

Max: 30 + 10log10(ChipRate/BitRate) + NormalizedPower dB

Sets the Eb/No of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:EBNO <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RACH:EBNO?