RCCCH

The Reverse Common Control Channel (RCCCH) is a portion of a Reverse CDMA Channel used for the transmission of digital control information from one or more mobile stations to a base station. The Reverse Common Control Channel can operate in the Reservation Access Mode. It can be power controlled and may support soft handoff.

1. General

2.Frame

State

Frame Length

Power

Frame Offset

Radio Configuration

EbNo

Data

 

Walsh Code

 

Walsh Code Length

 

Bit Rate

 

Channel Coding

 

BER Insertion

 

FER Insertion

 

Buttons

This button sets all channels to equal power, and the total power to 0 dB.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:PADJust EQUal|SCALe

This button scales all of the current channel powers so that the total power equals 0 dB, keeping the previous power ratios between the individual channels.

Click the Closedbutton to display the Code Domain Power (CDP) graph. This graph shows the position and power level of each channel, relative to the Walsh Code applied. After clicking this button, the button name changes to Hide Graph.

Click the button to close the graph. After clicking this button, the button name changes to Show Graph.

1. General

State

Choice: On | Off

Set operating state of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh[:STATe] ON|OFF|1|0

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh[:STATe]?

Power

Range: -40 to 0 dB

Set the power of the channel in dB.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:POWer <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:POWer?

Radio Configuration

Choice: 3 | 4

Set the Radio Configuration of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:RCONfig 3|4

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:RCONfig?

Data

Choice: PN9 | PN15 | Pattern | UserFile

Default: PN9

Edit the data pattern for the Reverse Fundamental Traffic Channel (RFCH) by clicking on the cell. Then click on the dialog box icon to launch the Closedselection dialog box.

Set the data of the channel. In the User File case, 0,1 txt file or binary file can be selected as the data source.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:DATA PN9|PN15|FIX4|"<file name>"

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:DATA?

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:DATA:FIX4 <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:DATA:FIX4?

Walsh Code

Display walsh code of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:WALSh?

Walsh Code Length

Display the walsh code length of the channel.

Bit Rate (bps)

Choice:

FrameLength = 5ms: 38400

FrameLength = 10ms: 19200 | 38400

FrameLength = 20ms: 9600 | 19200 | 38400

Set the bit rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:RATE 9.6kbps|19.2kbps|38.4kbps

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:RATE?

Channel Coding

Choice: All On | All Off

Set the channel code state of the channel.

If the coding state is off, the channel will be no channel coding and interleaver.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCH:CCODing ON|OFF|0|1

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:CCONtrol:RCCCH:CCODing?

BER Insertion

Range: 0% to 50%

Set the bit error rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCH:BER <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCH:BER?

FER Insertion

Range: 0% to 100%

Set the frame error rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCH:FER <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCH:FER?

2.Frame

Frame Length (ms)

Choice: 5 | 10 | 20

Set the frame Length of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:FLENgth 5|10|20

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:FLENgth?

Frame Offset (ms)

Choice:

Frame Length = 5ms: Range: 0 to 3

Frame Length = 10ms: Range: 0 to 7

Frame Length = 20ms: Range: 0 to 15

Frame Length = 40ms: Range: 0 to 31

Frame Length = 80ms: Range: 0 to 63

Set the frame offset of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:FOFFset <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:FOFFset?

EbNo

Range:

Min: -30 + 10log10(ChipRate/BitRate) + NormalizedPower dB

Max: 30 + 10log10(ChipRate/BitRate) + NormalizedPower dB

Set the Eb/No of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:EBNO <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:CCONtrol:RCCCh:EBNO?