RDCCH

The RDCCH (Reverse Dedicated Control Channel) is used for the transmission of higher-level data and control information from a mobile station to a base station.

1. General

2.Frame

State

Frame Length

Power

Frame Offset

Radio Configuration

EbNo

Data

 

Walsh Code

 

Walsh Code Length

 

Bit Rate

 

Channel Coding

 

BER Insertion

 

FER Insertion

 

Buttons

This button sets all channels to equal power, and the total power to 0 dB.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:PADJust EQUal|SCALe

This button scales all of the current channel powers so that the total power equals 0 dB, keeping the previous power ratios between the individual channels.

Click the Closedbutton to display the Code Domain Power (CDP) graph. This graph shows the position and power level of each channel, relative to the Walsh Code applied. After clicking this button, the button name changes to Hide Graph.

Click the button to close the graph. After clicking this button, the button name changes to Show Graph.

1. General

State

Choice: On | Off

Sets the operating state of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh[:STATe] ON|OFF|1|0

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh[:STATe]?

Power

Range: -40 to 0 dB

Sets the power of the channel in dB.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:POWer <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:POWer?

Radio Configuration

Choice: 3 | 4

Sets the Radio Configuration of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:RCONfig 3|4

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:RCONfig?

Data

Choice: PN9 | PN15 | Custome Bit Pattern | User File

Default: PN9

Edit the data pattern for the Reverse Fundamental Traffic Channel (RDCCH) by clicking on the cell. Then click on the dialog box icon to launch the Closedselection dialog box.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:DATA PN9|PN15|FIX4|"<file name>"

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:DATA?

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:DATA:FIX4 <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:DATA:FIX4?

Walsh Code

Display walsh code of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:WALSh?

Walsh Code Length

Display the walsh code length of the channel.

Bit Rate (bps)

Display the bit rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:RATE?

Channel Coding

Choice: All On | All Off

Sets the channel code state of the channel.

If the coding state is off, the channel will be no channel coding and interleaver.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:CCODing ON|OFF|0|1

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:CCODing?

BER Insertion

Range: 0% to 50%

Sets the bit error rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:BER <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:BER?

FER Insertion

Range: 0% to 100%

Sets the frame error rate of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:FER <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:FER?

2.Frame

Frame Length (ms)

Choice: 5 | 20

Sets the frame Length of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:FLENgth 5|20

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:FLENgth?

Frame Offset (ms)

Choice:

Frame Length = 5ms: Range: 0 to 3

Frame Length = 10ms: Range: 0 to 7

Frame Length = 20ms: Range: 0 to 15

Frame Length = 40ms: Range: 0 to 31

Frame Length = 80ms: Range: 0 to 63

Sets the frame offset of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:FOFFset <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC34:TRAFfic:RDCCh:FOFFset?

EbNo

Range:

Min: -30 + 10log10(ChipRate/BitRate) + NormalizedPower dB

Max: 30 + 10log10(ChipRate/BitRate) + NormalizedPower dB

Sets the Eb/No of the channel.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RSCH:EBNO <val>

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:RC12:ACCess:RSCH:EBNO?