Before installing the license file, save a backup copy in a safe place.
This topic supports N5172B EXG, N5182B MXG, and N5182A MXG vector signal generators.
To install the license file in your signal generator, follow one of the procedures below.
If your signal generator is connected to LAN, see Using Keysight License Manager.
If your signal generator is not connected to LAN, see Using a USB Storage Device or Using GPIB and SCPI Commands.
The Keysight License Manager software requires a LAN connection between the PC on which it is installed and the MXG/EXG signal generator. If your equipment cannot be connected through a LAN, install the license using a USB storage device.
If you do not have Keysight License Manager installed on your PC, you can download it at no charge from the following website: http://www.keysight.com/find/licensemanager.
Establish a LAN connection between the PC and the MXG/EXG signal generator, as described in Equipment Setup and Connection.
Copy the license file to your PC. The license file has a .lic extension, and is attached to the email message you received when you redeemed your license. In this example, the license file N5182A-US70000628.lic is placed in a folder named N5182A.
Obtain the hostname or IP address of your signal generator. Press
> > on the signal generator front panel. The hostname and IP address are displayed, as shown below.
On your PC, start the Keysight License Manager software. Click
> > > .In the Keysight License Manager main window, click
> to open the Connect to host system(s) dialog box.
In the
field, enter either the hostname or the IP address of the signal generator obtained in Step 4.Click drop-down figure.)
Click
> to open the Install License File(s) dialog box.Use the Install License File(s) dialog box to navigate to the location where you placed the license file (*.lic) in Step 3.
Select the desired license file and click
.Wait for a message to appear, informing you that the license has been successfully installed in the signal generator.
Refer to the Keysight License Manager online help for more information about using the software.
If you are unable to establish a LAN connection between your PC and your MXG/EXG signal generator, you can manually install the license using a USB storage device.
Copy the license file to a supported USB storage device. The license file is attached to the email message you received when you redeemed your license.
Insert the storage device into the USB port on the front panel of the MXG/EXG signal generator.
Press the
key to copy the file to the signal generator's memory.Cycle the signal generator power.
If you are unable to establish a LAN connection between your PC and your signal generator, you can manually install the license using a GPIB connection and the Keysight Connection Expert software (or another command line tool).
This method can be used for perpetual licenses only. To install or move a transportable license, you must use the Keysight License Manager software on a PC connected to your signal generator through LAN.
Copy the license file to your PC. The license file is attached to the email message your received when you redeemed your license.
On your PC, start the Keysight Connection Expert software. Click www.keysight.com/find/iolib.
> > . If you do not have Keysight IO Libraries Suite installed on your PC, you can download it fromIf you are not using Keysight Connection Expert, start your command line tool and proceed to step 5.
Select your signal generator, as shown below. If there are a lot of instruments connected to the network, you can use the Filter Instruments field to narrow your search.
Click
to open the Keysight Interactive IO window.
Open the license file you copied to your PC in Step 1 using Microsoft Notepad, or a similar text editor that creates plain, ASCII text files. Do not use a word processor such as Microsoft Word.
Using the text editor, select and copy the license file text.
Type the following SCPI command into the
field in the Keysight Interactive IO window, pasting the license file text you copied in Step 7 at the <license_line> location in the command.:SYST:LIC:INST "<license_line>"
Click the
button to send the command, or the button to send the command and read the response in the Instrument Session History displayed at the bottom of the window.