A transportable license can be moved from one instrument to another up to 10 times per month, but can be used on only one instrument at a time. This topic describes two methods for moving a transportable license between instruments.
Transporting a license requires the Keysight License Manager (ALM) software. If you do not have the Keysight License Manager installed on your PC, download it from the following website: www.keysight.com/find/licensemanager.
Make sure the source (currently licensed) instrument, the target instrument, and PC are connected to a LAN with Internet access.
Open the ALM software.
Click > . to open the Connect to Device dialog box.
In the Device Address field, enter either the hostname or the IP address of the source instrument.
Click . The
instrument hostname/address and its installed licenses appear in the tree
view (left pane). The right pane displays additional information for each
license. (See the
drop-down figure.)
Repeat steps 3 through 5 for the target instrument.
In the tree view, expand the Installed Licenses node of the source instrument. All the licenses used by that instrument are displayed.
From this list of licenses, find all the capability and connectivity licenses associated with the software model you want to move.
Drag and drop each of these licenses to the hostname/address node of the target instrument.
Configure a direct LAN connection between the PC and source (currently licensed) instrument. At this point, the PC does not require an Internet connection.
Open the ALM software.
In the tree view, delete the transportable license from the source instrument (either right-click the license and then select , or select the license and then press the Delete key).
A Transport License dialog box appears. In the dialog box, save the license contents to a file with a .url extension (for redemption later).
If you do not immediately save the license contents to a file, you can later retrieve the license contents in the Application Category of the Windows Event Viewer and use the contents for re-issue on the Keysight Software License Transportation web page: www.keysight.com/find/transportlicense.
Skip this step if your PC is connected to the Internet.
Copy the .url file you created in the previous step to a portable mass storage device, such as a USB flash drive.
Connect the portable mass storage device to a PC that is connected to the Internet.
From Windows Explorer, locate and double-click the .url file on the PC (or portable mass storage device). The .url file appears in a browser that is connected to the Keysight Software License Transportation web page. The fields automatically update with the license contents.
Enter the target instrument's hostid (model number, serial number) and then click the button. A link to the re-issued license is displayed.
Right-click the link and select . Save the license file to a location on your PC (or portable mass storage device).
Configure a direct LAN connection between the PC and target instrument.
Skip this step if your PC is connected to the Internet.
Connect the portable mass storage device to the PC that is connected to the target instrument.
Open the ALM software and select the target system in the tree view.
From Windows Explorer, locate the license file and drag (or copy and paste) it into ALM's tree view.