TCH/AFS 4.75k, TCH/AFS 5.15k, ...TCH/AFS 10.2k, TCH/AFS 12.2k are coded channels that are available with Option QFP. To open the Data node, click Data in the tree view. Use the Data window to define the bits in the bursts. The cells displayed in the Data node are determined by the Channel Type, as defined in the Timeslot window, for the selected timeslot.
The timeslots shown below are set to show some of the available timeslot (channel) types, not to show a typical test configuration.
Figure: Coded TCH/AFS 4.75k, TCH/AFS 5.15k, TCH/AFS 5.9k, TCH/AFS 6.7k, TCH/AFS 7.4k, TCH/AFS 7.95k, TCH/AFS 10.2k, and TCH/AFS 12.2k Data Node
|
1. Data (Normal GMSK Burst) |
|---|
|
2. Control Frame |
Click
to display a drop-down menu in which you can copy a timeslot configuration
from one timeslot to another.
Use the Data window to define the bits in the bursts. The cells displayed in the Data section are determined by the burst type (Timeslot Type) for the selected timeslot as defined in the Timeslots window. In the window shown above, Timeslots 0 is set up for a data cell with a coded adaptive multi-rate full rate speech traffic channel (TCH/AFS n.nK) bursts. (The image above, is specifically for the , but the other data node screens are similar.)
Tail bits are set by the software. This cell is not editable.
Click the Details button
in this cell to open the
Data Source
Selection
window.
Select an encoded , or . The selected data is coded continuously across the RLC data block per the 3GPP standards. An independent version of the selected data is coded across the MAC header.
To perform a receiver test with a continuous PN sequence, select .
You can enter 1 (control channel burst) or 0 (data channel burst). The default is 0.
Default: TSCO
Click the Details button
in this cell to open the
Data Source Selection
window.
Select to or to use for the training sequence bits.
If you manually change a timeslot (channel type), the training sequence for that timeslot resets to provided that the training sequence was not previously changed for the new channel type.
The training sequences selections are defined as follows:
|
TSC0 |
0970897 |
|
TSC1 |
0B778B7 |
|
TSC2 |
10EE90E |
|
TSC3 |
11ED11E |
|
TSC4 |
06B906B |
|
TSC5 |
13AC13A |
|
TSC6 |
29F629F |
|
TSC7 |
3BC4BBC |
Select to define
custom training sequence
bits.
Guard period bits are set by the software. This cell is not editable.
Figure: Guard Period Lengths Between Different Timeslots
|
Burst Transition |
Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods) |
|
|---|---|---|
|
TS0 and TS1 or TS4 and TS5 |
Any other timeslot pair |
|
|
normal symbol period to normal symbol period |
9 |
8 |
Choice: Independent | Consecutive data with Subjective Ordering | Consecutive data without Subjective Ordering
Default: Independent
Double-click or use the drop-down menu to set the
data placement type.
Refer to 3GPP TS 45.003-600, section 3.1 and Table 2; and 3GPP TS 46.010,
sections 3.1.1 to 3.1.4.
Choice: CODEC_MODE_1 (00) | CODEC_MODE_2 (01) | CODEC_MODE_3 (10) | CODEC_MODE_4 (11)
Default: CODEC_MODE_1
Double-click or use the drop-down menu to set the
In-band Data. Value of the
CODEC data
varies according to the AMR (Adaptive Mulit-Rate) Active Code Set (ACS).
Refer to 3GPP TS 45009-620, section 3.4.1.
Set the data for the control frame within a multiframe
setup. Click the Details button
in this cell to open the
Data Source Selection
window.
Select ,
or . Select , to
create
a data string.
If the Multiframe type parameter at the Carrier n node is set to , the parameter, while appearing as active, has no effect since there is no control frame.