Timeslot-based Waveform Setup 1 2 3 4 5 6

EDGE Measurements

Set the software to its initial state.

Press the New icon or select New from the File menu.

Enter a Waveform Name and Comment (optional)

  1. In the tree view, select Waveform Setup.

  2. Double-click the Waveform Name field in the Basic section and enter a name for the waveform.

  3. Double-click the Comment field in the Basic section and enter a comment to associate with the waveform.

Set the ARFCN and Transmit Device

  1. Set ARFCN to 1 as shown below

  2. Set Transmit Device to Base as shown below.

Select a Pre-defined Carrier Configuration

  1. In the tree view, select WFM1.

  2. Click the predefined configuration button , located above the summary table. 

  3. From the Pre-defined Carrier Configuration list that appears, select EDGE 1 Timeslot, 1 Carrier.

  4. Select Ok.

The selected predefined carrier appears in the carrier configuration summary table.

Use default instrument settings and Carrier settings.

Generate and Download the Waveform

Click the Generate and Download icon as shown below.

Measure the Signal

Measure the signal using an Keysight E4406A vector signal analyzer. Refer to EDGE Measurements in Keysight Literature number 5988-2389EN for instructions.