Frequency Bands and ARFCN

The following table shows the relationship between frequency band, ARFCN, and frequency.

For more information go to http://wireless.keysight.com/rfcomms/refdocs/gsmgprs/gen_bse_cell_band.php

Frequency Band

Uplink/Downlink Separation

Uplink Frequency Range (Transmit Device = Mobile)

Downlink Frequency Range (Transmit Device = Base)

ARFCN

GSM 450

10 MHz

450.4 to 457.6 MHz

460.4 to 467.6 MHz

259 to 293

GSM 480

10 MHz

478.8 to 486 MHz

488.8 to 496 MHz

306 to 340

GSM 750

30 MHz

747 to 762 MHz

777 to 792 MHz

438 to 511

GSM 850

45 MHz

824 to 849 MHz

869 to 894 MHz

128 to 251

P-GSM 900

45 MHz

890 to 915 MHz

935 to 960 MHz

1 to124

E-GSM 900

45 MHz

880 to 915 MHz

925 to 960 MHz

0 to124

and

975 to 1023

R-GSM 900

45 MHz

876 to 915 MHz

921 to 960 MHz

0 to124

and

955 to 1023

DCS 1800

45 MHz

1710 to 1785 MHz

1805 to 1880 MHz

512 to 885

PCS 1900

45 MHz

1850 to 1910 MHz

1930 to 1990 MHz

512 to 810

The examples below show how the software sets the frequency after you enter the Frequency Band, the ARFCN, and select Mobile or Base as the Transmit Device.

In the figure below, the P-GSM 900 frequency band is selected with Base as the Transmit Device. The corresponding frequency range from the table is 935 to 960 MHz. The entry of 124 forARFCN causes the software to set the frequency at the upper limit of the frequency range for Base (959.8 MHz).

Click the Generate Waveform button to update the frequency setting.

In the example below, the ARFCN is set to 1. The Frequency Band remains set at P-GSM 900 and Transmit Device remains set at Base. When the waveform is generated, the software sets the frequency to the lower limit of the frequency range for Base (935.2 MHz).

Waveform Setup