Continuous Pattern Configuration

State

Choice: On | Off

Default: On

Double-click or use the drop-down menu to set the state of the timeslot On or Off.

Power

Range: –70 to 0 dB.

Default: 0 dB

Enter a value to set the timeslot power.

Data

View the data type. The data type is set by the software. You cannot edit this cell.

Data Offset

Range: 0 to 32767

Default: 0

Enter a data offset value to use when generating the data stream.

Modulation

View the modulation type.

You cannot edit this cell.

CCDF Plot