To open the Data node, click Data in the tree view. The figure below shows the Data node.
|
1. Data (Access Burst) |
|---|
Click
to display a drop-down menu in which you can copy a timeslot configuration
from one timeslot to another.
Use the Data window to define the bits in the bursts. The cells displayed in the Data section are determined by the burst type (Timeslot Type) for the selected timeslot as defined in the Timeslots window. In the window shown above, Timeslot 0 is selected, so the data cells provided are for setting up an Access Burst.
Default: X"3A"
Enter 8 bits to use in the extended tail bit segment of the Access Burst.
Default: X"096FF335478"
Enter 41 bits to use for the synchronized sequence bits of the Access Burst.
Choice: PN9 | PN15 | User Defined Bits
Default: PN9
Click the Details button
in this cell to open the
Data Source Selection
window.
Select , or to use for the encrypted bits.
Select , to create an encrypted data string. (See the
drop-down figure.)
Tail bits are set by the software at 000. You cannot edit this cell.
The Extended Guard Period bits are set by the software. You cannot edit this cell.