This TDMA Frame description is for the carrier configuration:
when in the n node, is selected and in the n node, the configuration is selected.51 multiframe on TS0, comprising 51 TDMA frames, is used to support broadcast, common control and stand alone dedicated control (SDCCH) --and their associated control-- channels.
This 51 multiframe waveform includes:
Broadcast Control Channel (BCCH)
Correction Control Channel (CCCH)
Synchronization Channel (SCH)
Frequency Correction Channel (FCCH) and
Idle burst
The BCH and CCH message data are setup as the same as the default setup for the 8960 Series 10 Wireless Communications Test Set.
In the .
In the drop down window click on
.In
the Add New Carrier button
and then click on .
The default is
.Refer to 3GPP TS 45.001 V7.7.0 (2008-02).
F: TDMA frame for frequency correction burst |
S: TDMA frame for synchronization burst |
B: TDMA frame for BCCH |
C: TDMA frame for CCCH |
D:TDMA frame for SDCCH |
A: TDMA frame for SACCH/C |
R: TDMA frame for RACH |
|
Figure: Channel Organization in the 51-frame multiframe