For EXT instrument problems, refer to the EXT's documentation.
Check the signal generator for error messages. If possible, correct the conditions indicated by the messages.
When a setting conflict (error) occurs, an error number and a brief message appear at the bottom of the signal generator display. You can view the full text of the error message on the signal generator front panel or by executing SCPI commands.
Front panel: Press the hardkey on the signal generator front panel to view error messages on the display.
SCPI: Execute the SCPI error commands described in the System Subsystem section of the SCPI Reference.
Refer to the signal generator documentation for further troubleshooting.
If necessary, contact Keysight Technologies.
Refer to the PXB's online documentation for error message descriptions and troubleshooting procedures.
This error is displayed when the PXB is not configured to accept an ARB waveform file or if not enough BBG resources are available. Check the following possible causes:
Confirm that you have loaded the correct configuration on the PXB.
Confirm that the loaded configuration contains the correct number of BBGs. For example, if Signal Studio set up to download two waveform files, the loaded PXB configuration must contain at least two BBGs.
You cannot download waveforms from Signal Studio to the PXB while the PXB is playing a waveform.
Press the “Stop” button on the PXB to stop the currently playing waveform before downloading waveforms from Signal Studio.
Verify that the equipment meets the minimum requirements, as described in the system requirements.
Refer to the computer's documentation for troubleshooting and repair.