Select in the tree view to display the window shown below. Refer to the Licensing topic for information about licensing and connectivity options.
Displays the licensed feature's index number.
Double-click or use the drop-down menu to set the operating state of the selected feature.
The State cell color changes to orange if a feature is set to and a valid license is not available.
If you set the state to for a licensed feature that is used in the current setup, a window opens that prompts you to save the current setup before continuing.
Displays the option number of the licensed feature.
|
Option Number |
Capability Type |
License Locked To: |
Time Based |
|---|---|---|---|
|
N7602B-Exx |
Basic GSM/EDGE capability |
Yes |
|
|
N7602B-Fxx |
Basic EGPRS2 capability (requires Exx) |
Target instrument serial number/bar code |
Yes |
|
N7602-QFP |
Advanced Capability for Control Channel |
Instrument serial number |
Yes |
|
Option Number |
Connectivity Type |
License Locked To: |
Time Based |
|---|---|---|---|
|
N7602B-1xx |
ESG connectivity |
Instrument serial number |
Yes |
|
N7602B-2xx |
PSG connectivity |
Instrument serial number |
Yes |
|
N7602B-3xx |
EXG/MXG connectivity |
Instrument serial number |
Yes |
|
N7602-6FP |
PXB connectivity |
Instrument serial number |
No |
|
N7602-8FP |
EXT connectivity |
Instrument serial number |
No |
Displays a description of the licensed feature.
The minor enhancement updates (MEU) option allows you to obtain the latest capabilities of the software. It is purchased as N7602B-MEU. However, each enhancement update is licensed as N7602B-Uxx, as shown in the image above. As more enhancements become available, the option suffix increments: U01, U02, U03 and so on. Purchasing MEU includes all the capabilities from previous MEU licenses. For example, purchasing the license for U03 includes everything that was in U01 and U02. If you had purchased an earlier MEU license, such as U01, and want the most recent MEU capabilities available in U03, purchasing another MEU license upgrades your software to the most current state.
Displays the status of the selected license on the connected instrument.
– the license is installed and active.
– the license is expired or not installed.
– the license is not applicable.
– Signal Studio software does not provide license information for some products.
When a new instrument connection is established or the hardware configuration is changed, the instrument licenses are automatically retrieved from the connected instrument. If the connected instrument does not have the correct licensing for the current waveform setup, initial settings are restored. You are prompted to save the setup parameters before continuing.
Displays the name of the carrier associated with the selected feature.
Displays the status of the carrier.
– the carrier is available for use.
– the carrier is not available or the license is not active.
Displays the name of the feature required for the selected instrument.