|
8PSK |
eight phase shift keying |
|
16QAM |
16 quadrature amplitude modulation |
|
32QAM |
32 quadrature amplitude modulation |
|
ALC |
automatic leveling control |
|
AN |
Access network. The network equipment providing data connectivity between a packet switched data network and the access terminals. An access network is equivalent to a base station. |
|
API |
application programming interface |
|
Arb |
arbitrary, as in arbitrary waveform |
|
ASCII |
American standard code for information interchange |
|
AT |
Access terminal. A device providing data connectivity to a user. An access terminal may be connected to a computing device such as a laptop personal computer or it may be a self-contained data device such as a personal digital assistant. An access terminal is equivalent to a mobile station. |
|
AWGN |
additive white Gaussian noise |
|
BBG |
baseband generator |
|
BER |
bit error rate |
|
BS |
base station |
|
BTTI |
basic transmission time interval |
|
Burst |
a specifically structured set of data bits that occupies a single timeslot in a TDMA frame. In GSM there are four types of bursts: normal, frequency correction, synchronous, and access. |
|
CCDF |
complementary cumulative distribution function |
|
CCITT |
Comité Consultatif International Téléphonique et Télégraphique |
|
Channel |
set of channels transmitted between the access network and the access terminals within a given frequency assignment. |
|
The signal generator transmits a continuous data stream without framing or bursting. |
|
|
A non-truncated PN9 sequence where all 511 bits are transmitted before the sequence repeats. |
|
|
dB |
decibels |
|
dBm |
decibels relative to 1 mW |
|
EDGE |
Enhanced Data Rates for GSM Evolution |
|
EGPRS2 |
Enhanced General Packet Radio Service 2 |
|
EXT |
Keysight E6607 EXT Wireless Communications Test Set |
|
FANR |
fast ack/nack reporting |
|
frame |
duration of time specified by 8 timeslots (4.6 ms) |
|
GMSK |
Gaussian minimum shift keying |
|
GPIB |
general purpose interface bus |
|
GSM |
Global System for Mobile Communications |
|
GUI |
graphical user interface |
|
HSR |
higher symbol rate |
|
I/O |
input/output |
|
IP address |
internet protocol address |
|
I/Q |
in-phase and quadrature channels |
|
LAN |
local area network |
|
marker |
a specific location on a waveform that can be configured to output a specified signal at a signal generator output port |
|
ms |
milliseconds |
|
MS |
mobile station |
|
MSB |
most significant bit |
|
PC |
personal computer |
|
PN |
pseudo-random number |
|
PXB |
Keysight N5106A PXB Baseband Generator and Channel Emulator |
|
OSR |
oversampling ratio |
|
QPSK |
quadrature phase shift keying |
|
Quick setup |
a saved configuration that includes software settings and instrument settings |
|
RF |
radio frequency |
|
RMS |
root mean square |
|
RTTI |
reduced transmission time interval |
|
SCPI |
standard commands for programmable instrumentation |
|
SS |
subscriber station (mobile) |
|
System Configuration Wizard |
a utility in the Signal Studio for GSM/EDGE software used for setting up the connection between the PC running the software and one or more instruments |
|
TDM |
time division multiplex or multiplexing |
|
TDMA |
time division multiple access |
|
TDMA frame |
duration of time specified by 8 timeslots (4.6 ms) |
|
Timeslot |
one of eight equal time divisions in a TDMA frame (0.577 ms) |
|
Tree view |
the left pane of the software's user interface |
|
TS |
training sequence |
|
UI |
user interface |