Use this topic to view the descriptions and SCPI commands for the node settings. To view the dialog box used with one of the settings, go to Dialog Boxes.
The node is available only when is the Data Format selection in the node.
Use the following links to navigate to and view the available settings:
Set the pattern type by clicking on the cell. Then click the dialog box icon
to launch the Data Setup dialog box.
[:SOURce]:RADio:EDGE[:BBG]:DATA PN9|PN11|PN15|PN20|PN23|PATTern|"<file name>"|EXT
[:SOURce]:RADio:EDGE[:BBG]:DATA?
If PATTern is the choice, use the following command to create the data pattern:
[:SOURce]:RADio:EDGE[:BBG]:DATA:PATTern "<bit_string>"
[:SOURce]:RADio:EDGE[:BBG]:DATA:PATTern?
Choices: GMSK | 8PSK and 3PI/8 rotation
Default: GMSK
Double click the cell, or click in the cell and use the drop-down menu to select the modulation type:
|
use this choice for a GSM signal |
|
use this choice for an EDGE signal |
[:SOURce]:RADio:EDGE[:BBG]:DATA:MODulation[:TYPE] MSK|PSK8
[:SOURce]:RADio:EDGE[:BBG]:DATA:MODulation[:TYPE]?
Range: 0–32767 symbols
Default: 0
Highlight the current value and enter a new number within the range.