Real-time data input is only used when AUX Operating Mode is .
There are 4 parameters for Real-time data input settings.
Real-time Data Input Pin1-3 defines which Aux Pin to used as data input.
Real-time Data Input Baud Rate defines the baud rate for UART timing. The 5 baud rate choices are: 115200, 230400, 460800, 576000, 921600.
For some cases, such as continuous GMSK modulation, you may not need 3 input pins. You can just use 1 or 2 pins and set other pin to “Unassigned” or keep the assigned pins open.
When using real-time data input, set Pattern Data in the Continuous node to .
The following figure shows using 3 Data Input pins in Aux IO. You can use 1, 2, or 3 Aux pins.
For GSM, you can just use one data input as shown below.