Real Time

Start Trigger

When Trigger Type is set to Continuous, and Continuous Type is set to Trigger & Run, the signal is played after the application is turned on and the first trigger edge is asserted.

(subsequent trigger signals are ignored)

Generated Pattern Marker and Frame Marker are two types output signal that can be assigned to one of marker outputs