Configuring for a Crossover LAN
To set up your system for a crossover LAN connection (direct connection between a PC and instrument), do the following:
Configure the PC
-
From your PC's Control Panel, double-click Network Connections > Local Area Connection.
-
In the Local Area Connection Properties dialog box, highlight Internet Protocol (TCP/IP). Ensure that the check box remains selected.
-
Click Properties.
-
Select Use the following IP address (radio selection).
-
Enter 1 once for each of the four areas that make up the IP address. After your entries, the IP address should show 1.1.1.1.
-
Click the Subnet mask entry field; an address appears.
-
Click OK to accept the configuration.
-
Close the Local Area Connection Properties dialog box.
-
Close the Network Connections window.
To Reconfigure for a LAN Connection
-
Reconnect the LAN cable.
-
From your PC's Control Panel, click Network Connections > Local Area Connection.
-
In the Local Area Connection Status dialog box, click Properties.
-
In the Local Area Connection Properties dialog box, highlight Internet Protocol (TCP/IP). Ensure that the check box remains selected.
-
Click Properties.
-
Select the Obtain an IP address automatically option or enter your system IP address.
-
Click OK to accept the configuration.
-
Close the Local Area Connection Properties dialog box.
-
Close the Local Area Connection Status dialog box and the Network Connections window.
Configure the Signal Generator
-
Turn on the signal generator.
-
Use the appropriate key-press sequence for the signal generator you are using:
EXG or MXG: Utility > I/O Config > LAN Setup > Manual Config Settings > IP Address
-
Record the current IP address.
-
Enter 1.1.1.2 as the new IP address.
-
Press Enter > Proceed with Reconfiguration > Confirm Change.
The signal generator reboots, completing the LAN reconfiguration.
Configuring Additional Instruments
To configure additional instruments, such as a spectrum analyzer, increment the IP address for each additional instrument by one. For example, use 1.1.1.3 as the IP address for a third instrument and 1.1.1.4 for a fourth instrument. Refer to the user documentation of the instrument you want to add for specific crossover configuration information.