7. Testing Connections

Installation Steps: 1 2 3 4 5 6 7

  1. Turn on the instrument and the computer.

  2. Start the Signal Studio software.

  3. Establish communications between the software and the instrument by first selecting New hardware configuration in the ClosedWelcome to Keysight Signal Studio... dialog box (System Configuration Wizard) that appears.

  4. Click OK and follow the remaining prompts. (Be prepared to enter the instrument's IP/GPIB address.)

    If you are running Signal Studio on a PC connected to a signal generator, refer to the following table to locate the instrument's address (LAN/GPIB) or hostname (LAN only):

    Connection

    Signal Generator

    Key Path

    LAN

    EXG and MXG1

    Utility > I/O Config > LAN Setup > Manual Config Settings

    GPIB

    EXG and MXG

    Utility > I/O Config > GPIB Setup

    1 Signal Studio accepts either the LAN address or hostname. So if you want to use the hostname, just enter the hostname into the software's Hostname/IP Address field.

    If the connection fails or for help with error messages, refer to Troubleshooting.

    After making the connection, you can view the instrument's information by selecting Hardware in the tree view.

  5. Install the software license (see Installing the License).