Hardware Settings
Click in the tree view to display read-only information about the system hardware. Expanding the node in the tree view reveals the node, which opens a window where you can change various instrument settings, such as frequency and amplitude.
For information about using the software to change instrument settings, go to the appropriate topic:
-
for waveform playback (Arb) software, see Instrument
When using a simulated signal generator connection, <Simulated Hardware> appears in the cell and <Simulated RF Signal Generator> appears in the cell. N/A appears in most of the other cells.
1. System Details
Name
View the name assigned to the system.
Description
View the hardware configuration type.
2. RF Signal Generator Details
Connection
View connection details (LAN or GPIB).
Model Number
View the instrument model number.
Serial Number
View the instrument serial number.
Firmware Revision
View the instrument firmware revision number.
2.1 Options
View the options of the connected instrument. These cells are not displayed when using simulated hardware.