Fader Channel Model - LTE
Base Station
The following predefined configurations are based on 3GPP TS 36.104 V8.2.0 (2008-05).
|
Carrier Frequency
(MHz) |
||
|---|---|---|
|
I |
2110 |
EPA, EVA, ETU |
|
II |
1930 |
EPA, EVA, ETU |
|
III |
1805 |
EPA, EVA, ETU |
|
IV |
2110 |
EPA, EVA, ETU |
|
V |
869 |
EPA, EVA, ETU |
|
VI |
875 |
EPA, EVA, ETU |
|
VII |
2620 |
EPA, EVA, ETU |
|
VIII |
925 |
EPA, EVA, ETU |
|
IX |
1844.9 |
EPA, EVA, ETU |
|
X |
2110 |
EPA, EVA, ETU |
|
XIII |
746 |
EPA, EVA, ETU |
Fading Profile
Select the delay profile to apply to the fading simulation. When you select a profile, the carrier frequency in fader setup and the path configuration will be updated according to the fading profile table selected.
|
Path # |
Doppler (Hz) |
Fading Type |
Delay (ns) |
Relative Loss (dB) |
|---|---|---|---|---|
|
1 |
5 |
Rayleigh |
0 |
0 |
|
2 |
5 |
Rayleigh |
30 |
1.0 |
|
3 |
5 |
Rayleigh |
70 |
2.0 |
|
4 |
5 |
Rayleigh |
90 |
3.0 |
|
5 |
5 |
Rayleigh |
110 |
8.0 |
|
6 |
5 |
Rayleigh |
190 |
17.2 |
|
7 |
5 |
Rayleigh |
410 |
20.8 |
|
Path # |
Doppler (Hz) |
Fading Type |
Delay (ns) |
Relative Loss (dB) |
|
1 |
70 |
Rayleigh |
0 |
0.0 |
|
2 |
70 |
Rayleigh |
30 |
1.5 |
|
3 |
70 |
Rayleigh |
150 |
1.4 |
|
4 |
70 |
Rayleigh |
310 |
13.6 |
|
5 |
70 |
Rayleigh |
370 |
0.6 |
|
6 |
70 |
Rayleigh |
710 |
9.1 |
|
7 |
70 |
Rayleigh |
1090 |
7.0 |
|
8 |
70 |
Rayleigh |
1730 |
12.0 |
|
9 |
70 |
Rayleigh |
2510 |
16.9 |
|
Path # |
Doppler (Hz) |
Fading Type |
Delay (ns) |
Relative Loss (dB) |
|
1 |
300 |
Rayleigh |
0 |
1.0 |
|
2 |
300 |
Rayleigh |
50 |
1.0 |
|
3 |
300 |
Rayleigh |
120 |
1.0 |
|
4 |
300 |
Rayleigh |
200 |
0.0 |
|
5 |
300 |
Rayleigh |
230 |
0.0 |
|
6 |
300 |
Rayleigh |
500 |
0.0 |
|
7 |
300 |
Rayleigh |
1600 |
3.0 |
|
8 |
300 |
Rayleigh |
2300 |
5.0 |
|
9 |
300 |
Rayleigh |
5000 |
7.0 |
Mobile Station
The following predefined configurations are based on 3GPP TS 36.104 V8.2.0 (2008-05).
|
Carrier Frequency
(MHz) |
||
|---|---|---|
|
I |
1920 |
EPA, EVA, ETU |
|
II |
1850 |
EPA, EVA, ETU |
|
III |
1710 |
EPA, EVA, ETU |
|
IV |
1710 |
EPA, EVA, ETU |
|
V |
824 |
EPA, EVA, ETU |
|
VI |
830 |
EPA, EVA, ETU |
|
VII |
2500 |
EPA, EVA, ETU |
|
VIII |
880 |
EPA, EVA, ETU |
|
IX |
1749.5 |
EPA, EVA, ETU |
|
X |
1710 |
EPA, EVA, ETU |
|
XIII |
777 |
EPA, EVA, ETU |
Fading Profile
Select the delay profile to apply to the fading simulation. When you select a profile, the carrier frequency in fader setup and the path configuration will be updated according to the fading profile table selected.
|
Path # |
Doppler (Hz) |
Fading Type |
Delay (ns) |
Relative Loss (dB) |
|
1 |
5 |
Rayleigh |
0 |
0 |
|
2 |
5 |
Rayleigh |
30 |
1.0 |
|
3 |
5 |
Rayleigh |
70 |
2.0 |
|
4 |
5 |
Rayleigh |
90 |
3.0 |
|
5 |
5 |
Rayleigh |
110 |
8.0 |
|
6 |
5 |
Rayleigh |
190 |
17.2 |
|
7 |
5 |
Rayleigh |
410 |
20.8 |
|
Path # |
Doppler (Hz) |
Fading Type |
Delay (ns) |
Relative Loss (dB) |
|
1 |
70 |
Rayleigh |
0 |
0.0 |
|
2 |
70 |
Rayleigh |
30 |
1.5 |
|
3 |
70 |
Rayleigh |
150 |
1.4 |
|
4 |
70 |
Rayleigh |
310 |
13.6 |
|
5 |
70 |
Rayleigh |
370 |
0.6 |
|
6 |
70 |
Rayleigh |
710 |
9.1 |
|
7 |
70 |
Rayleigh |
1090 |
7.0 |
|
8 |
70 |
Rayleigh |
1730 |
12.0 |
|
9 |
70 |
Rayleigh |
2510 |
16.9 |
|
Path # |
Doppler (Hz) |
Fading Type |
Delay (ns) |
Relative Loss (dB) |
|
1 |
300 |
Rayleigh |
0 |
1.0 |
|
2 |
300 |
Rayleigh |
50 |
1.0 |
|
3 |
300 |
Rayleigh |
120 |
1.0 |
|
4 |
300 |
Rayleigh |
200 |
0.0 |
|
5 |
300 |
Rayleigh |
230 |
0.0 |
|
6 |
300 |
Rayleigh |
500 |
0.0 |
|
7 |
300 |
Rayleigh |
1600 |
3.0 |
|
8 |
300 |
Rayleigh |
2300 |
5.0 |
|
9 |
300 |
Rayleigh |
5000 |
7.0 |
High Speed Train
The high speed train condition for open space and tunnel are non-fading propagation channels with one tap and is a special very high mobility case as specified in 3GPP TS 36.104 V8.2.0 (2008-05).
The high speed train condition for leaky cable is a fading propagation channel with one path (tap). The Rician K factor is the ratio between the dominant signal power and the variant of other weaker signals.
Fading Profile
|
Parameter |
|||
|---|---|---|---|
|
Ds |
1000 m |
300 m |
Infinity |
|
Dmin |
50 m |
2 m |
-– |
|
K |
|
|
10 dB |
|
v |
350 km/h |
300 km/h |
300 km/h |
|
fd |
1340 Hz |
1150 Hz |
1150 Hz |
Moving Propagation
The LTE Moving Propagation condition tests
a receiver’s ability to adjust to changing delay conditions. The
ETU200 profile uses multiple paths (taps) and is based on a 200 Hz doppler
frequency.
Illustration...
The AWGN Only profile uses a single path with a doppler frequency of 622.653 Hz.
When you select Moving Propagation as the fader profile, Delay, Min Delay, Max Delay and Rate of Oscillation can be set in the fader path columns.
Fading Profile
|
Parameter |
ETU 200 |
AWGN Only |
|---|---|---|
|
UE speed |
120 km/h |
350 km/h |
|
CP length |
Normal |
Normal |
|
|
|
|
|
A |
10 µs |
10 µs |
|
|
0.04 s-1 |
0.13 s-1 |