Real Time

Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to topic Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Fading

1. Fader Settings

Fader Channel Model

Use the drop-down menu to select a default or standards-based fading model. The standard models cover SISO propagation environments that allow you to test whether your device meets the performance requirements as defined by the respective standard. The software automatically populates the path configurations for the selected standard model.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:SCModel DEFault|<SISO_Channel_Model_Name>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:SCModel?

Click the links below to see the SCPI syntax for executing the various SISO fading models. The syntax for each fading model appears in the exact same order (top to bottom) as the software's GUI, allowing you to compare and confirm you have the correct syntax for the fading model you want to execute.

Closedcdma2000

CDMABS1

CDMABS2

CDMABS3

CDMABS4

CDMAMS1

CDMAMS21

CDMAMS22

CDMAMS3

CDMAMS4

CDMAMS5

CDMAMS6

ClosedW-CDMA

WCDMABS1

WCDMABS2

WCDMABS3

WCDMABS4

WCDMABSBD

WCDMABSMP

WCDMAMS1

WCDMAMS2

WCDMAMS3

WCDMAMS4

WCDMAMS5

WCDMAMS6

WCDMAMSBD

WCDMAMSMP

WCDMAHSTT

WCDMAHSTO

WCDMAHSTLC

ClosedGSM/EDGE

GERA1

GERA2

GEHT12T1

GEHT12T2

GEHT6T1

GEHT6T2

GETU12T1

GETU12T2

GETU6T1

GETU6T2

GEEQ

GETI

ClosedCOST 259

C259TU

C259RA

C259HT

ClosedWLAN

WLANA

WLANB

WLANC

WLAND

WLANE

Closed1xEV-DO

XEV11

XEV12

XEV21

XEV22

XEV31

XEV32

XEV41

XEV42

XEV5

ClosedTD-SCDMA

TDSCDMA1

TDSCDMA2

TDSCDMA3

ClosedcdmaOne

CDMAONE1

CDMAONE21

CDMAONE22

CDMAONE3

CDMAONE4

CDMAONE5

ClosedHSDPA

HSDPAC13

HSDPAC17

HSDPAC12

HSDPAC14

HSDPAC18

HSDPAC23

HSDPAC27

HSDPAC22

HSDPAC24

HSDPAC28

HSDPAC33

HSDPAC37

HSDPAC32

HSDPAC34

HSDPAC38

HSDPAC43

HSDPAC47

HSDPAC42

HSDPAC44

HSDPAC48

HSDPAC53

HSDPAC57

HSDPAC52

HSDPAC54

HSDPAC58

HSDPAC63

HSDPAC67

HSDPAC62

HSDPAC64

HSDPAC68

HSDPAC83

HSDPAC87

HSDPAC82

HSDPAC84

HSDPAC88

HSDPAPA3

HSDPAPA7

HSDPAPA2

HSDPAPA4

HSDPAPA8

HSDPAPB3

HSDPAPB7

HSDPAPB2

HSDPAPB4

HSDPAPB8

HSDPAVA30

HSDPAVA71

HSDPAVA23

HSDPAVA120

HSDPAVA282

HSDPAVA92

HSDPAVA41

HSDPACVA80

HSDPAVA166

HSDPAVA320

ClosedHSUPA

HSUPAC13

HSUPAC17

HSUPAC12

HSUPAC23

HSUPAC27

HSUPAC22

HSUPAC33

HSUPAC37

HSUPAC32

HSUPAC43

HSUPAC47

HSUPAC42

HSUPAPA3

HSUPAPA7

HSUPAPA2

HSUPAPB3

HSUPAPB7

HSUPAPB2

HSUPAVA30

HSUPAVA71

HSUPAVA23

HSUPAVA120

HSUPAVA282

HSUPAVA92

ClosedHSPA

HSPAHSTT

HSPAHSTO

HSPAHSTLC

ClosedTETRA

TETRAS

TETRAR

TETRAT

TETRAB

TETRAH

TETRAE

ClosedLTE

LTEBS1EPA

LTEBS1EVA

LTEBS1ETU

LTEBS2EPA

LTEBS2EVA

LTEBS2ETU

LTEBS3EPA

LTEBS3EVA

LTEBS3ETU

LTEBS4EPA

LTEBS4EVA

LTEBS4ETU

LTEBS5EPA

LTEBS5EVA

LTEBS5ETU

LTEBS6EPA

LTEBS6EVA

LTEBS6ETU

LTEBS7EPA

LTEBS7EVA

LTEBS7ETU

LTEBS8EPA

LTEBS8EVA

LTEBS8ETU

LTEBS9EPA

LTEBS9EVA

LTEBS9ETU

LTEBS10EPA

LTEBS10EVA

LTEBS10ETU

LTEBS13EPA

LTEBS13EVA

LTEBS13ETU

LTEMS1EPA

LTEMS1EVA

LTEMS1ETU

LTEMS2EPA

LTEMS2EVA

LTEMS2ETU

LTEMS3EPA

LTEMS3EVA

LTEMS3ETU

LTEMS4EPA

LTEMS4EVA

LTEMS4ETU

LTEMS5EPA

LTEMS5EVA

LTEMS5ETU

LTEMS6EPA

LTEMS6EVA

LTEMS6ETU

LTEMS7EPA

LTEMS7EVA

LTEMS7ETU

LTEMS8EPA

LTEMS8EVA

LTEMS8ETU

LTEMS9EPA

LTEMS9EVA

LTEMS9ETU

LTEMS10EPA

LTEMS10EVA

LTEMS10ETU

LTEMS13EPA

LTEMS13EVA

LTEMS13ETU

LTEHSTO

LTEHSTT

LTEMPETU

LTEMPAWGN

LTEHSTLC

ClosedDVB

DVBTP16

DVBHPI

DVBHPO

DVBTMTU6

DVBHSFNWLE

DVBHSFNSLE

DVBHSFNSSE

ClosedAPCO25

APCOFRS1

APCOFRS2

APCODSC

Closed802.11p

IEEE11PRLOS

IEEE11PUALOS

IEEE11PCNLOS

IEEE11PHLOS

IEEE11PHNLOS

Carrier Frequency

Default: 1.0 GHz

Range: 1 to 44 GHz

Sets the carrier frequency to be used for Doppler effects in the fading simulations. The Carrier Frequency setting is coupled with the Frequency setting under the Instrument node. Also if you change the Carrier Frequency value, the Doppler Frequency or the Vehicle Speed settings under the Fader Path node will be changed.

When using SCPI, the instrument frequency and carrier frequency settings are not coupled, as they are when using the GUI. Therefore you must send separate commands to ensure both are the same. Also, you must repeat these commands each time you set the fader channel model because some models change the carrier frequency, but not the instrument frequency.

Example:

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:SCModel IEEE11PRLOS (sets fader channel model)

[:SOURce]:FSIMulator[1]:FADer[1]:FREQuency 5.86GHz (sets carrier frequency)

:FREQ 5.86GHz (sets instrument frequency)

[:SOURce]:FSIMulator[1]:FADer[1]:FREQuency <val>

[:SOURce]:FSIMulator[1]:FADer[1]:FREQuency?

1. Fader Settings - Birth-Death

These parameters apply to the following fading models only. In addition, for the associated SCPI command to be valid, one of these fading models must be executed first. See Fader Channel Model.

Minimum Delay

Range: -100 ns to -25 us

Default: -5 us

Minimum Delay sets the minimum birth-death path delay when you select a Birth-Death delay profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MINDelay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MINDelay?

Maximum Delay

Range: 100 ns to 25 us

Default: 5 us

Maximum Delay sets the maximum birth-death path delay when you select a Birth-Death delay profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MAXDelay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:MAXDelay?

Delay Bin Spacing

Range: 100 ns to 5 us

Default: 1 us

Delay Bin Spacing sets the size of the radom hops when you select a Birth-Death delay profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DBSPacing <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DBSPacing?

Dwell Time

Range: 0.1 s to 1.0 s

Default: 191 ms

Dwell Time sets the duration of each birth-death state when you select a Birth-Death delay profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DTIMe <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:DTIMe?

1. Fader Settings - High Speed Train

These parameters apply to the following fading models only. In addition, for the associated SCPI command to be valid, one of these fading models must be executed first. See Fader Channel Model.

Base Station Initial Distance (Ds/2)

Range: 5 m to 50 km

Default: Varies by channel model

Sets the initial distance (Ds/2) that the mobile must travel before passing the base station when you select a high speed train profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSIDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSIDistance?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSIDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSIDistance?

Base Station Minimum Distance (Dmin)

Range: 1 m to 1 km

Default: Varies by channel model

Sets the minimum distance from the mobile to the base station (BS-Railway track distance) when you select a high speed train profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSMDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:BSMDistance?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSMDistance <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:BSMDistance?

Train Speed

Range: 0 to 1000 km/h

Default: Varies by channel model

Sets the speed of the train when you select a high speed train profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:TSPeed <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANDard:WCDMa:HSTrain:TSPeed?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:TSPeed <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANDard:LTE:HSTrain:TSPeed?

Maximum Doppler Frequency

Range: 0 to 1.6 kHz

Default: Varies by channel model

Sets the maximum Doppler frequency for the fading simulation when you select a high speed train profile.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:MDFRequency <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:WCDMa:HSTrain:MDFRequency?

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:MDFRequency <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:LTE:HSTrain:MDFRequency?

1. Fader Settings - DVB

These parameters apply to the following fading models only. In addition, for the associated SCPI command to be valid, one of these fading models must be executed first. See Fader Channel Model.

Echo Delay

Range: 0 to 1 ms

Default: Varies by channel model

Sets the additional delay for DVB fading paths 7-12 that are part of the echo.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:EDELay <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:EDELay?

Echo Loss

Range: 0 to 20 dB

Default: Varies by channel model

Sets the additional loss for DVB fading path 7-12 that are part of the echo.

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:ELOSs <val>

[:SOURce]:FSIMulator[1]:FADer[1]:STANdard:ELOSs?

2. Random Seed

Random Seed

Range: 0 to 2^89 – 1

Sets the random number generation seed of the fading channel. If it is set to zero, the generated fading will be different for each playback to provide randomness for each test. To reproduce the same fading environment for the same configuration as the last time it was played, use the same seed value (other than 0) each time.

You can enter the entire 89-bit sequence directly into the random seed cell or use the high, medium, and low cells to designate the number in three segments for easier data entry.

[:SOURce]:FSIMulator[1]:SEED "<val>"

[:SOURce]:FSIMulator[1]:SEED?

Low (Hex)

Specifies the lowest bits (0x0 to 0xFFFFFFFF).

Middle (Hex)

Specifies the middle bits (0x0 to 0xFFFFFFFF).

High (Hex)

Specifies the upper bits (0x0 to 0x1FFFFFF).