Frequency Hopping

The following example procedure shows how to create waveforms with frequency hopping.

  1. Select Bluetooth Basic Rate + Enhanced Rate from the Format drop-down menu.

  2. Click Packet in the tree view on the left to configure the packet parameters.

    Set Payload Distribution to Multiple Packets.   

    Set LAP to 0x000000   

  3. Click Bluetooth BR+EDR in the tree view on the left to configure the Bluetooth parameters.

    Set Frequency Hopping State to On.    

    Set CLK Start to 0x0000010.    

     

  4. Click the in the tool bar to generate and download the waveform to the signal generator.