Go to topic Go to description Go to description Go to description Go to description Go to topic Go to topic Go to description

2. Coding and Modulation

Coding State

Choice: On | Off

Default: Off

Specify the coding state of LE radio.

Coding Indicator

Range: 0 ~ 1

Default: 0

Set the coding indicator of LE radio.

Modulation Index

Range: 0.45 to 0.55

Default: 0.5

Double-click or use the drop-down menu to enter the modulation index of GFSK.

BT

Range: 0.1 to 2.0

Default: 0.1

Enter the BT product of the Gaussian filter.

Symbol Rate

Choice: 1 Ms/s | 2 Ms/s

Default: 1 Ms/s

Double-click or use the drop-down menu to select the Symbol Rate of LE radio.

2 Mb/s LE is a feature of BLE 5.0., it requires the LE physical layer to support 2Ms/s packets to be transmitted.