Select in the
tree view
to display a list of waveform setups, each of which is associated with
a specific user-defined hardware configuration or a predefined hardware
configuration (Sim HW).
Quick setups are accessible only from the Quick Setup node in the user interface. To save your waveform setup as a file that can be shared with other users, use > or > .
Signal Studio software provides predefined quick setups that enable you to examine the default parameters for a particular function, while in simulated hardware mode. You can use the predefined quick setups as a starting point, modify the settings as desired, then save them as a new quick setup (see Custom Quick Setup). However, you cannot modify or delete the predefined quick setups.
After you have defined waveform parameters in the Instrument node and the Waveform Setup node, you can associate this waveform setup with the currently configured hardware (displayed in the Hardware node) by pressing the button and providing a name for the new Quick Setup.
To save the current waveform setup with a different hardware configuration, define the new hardware configuration using the System Configuration Wizard ( > ), then click .
If you change one or more Waveform Setup parameters, the software prompts you to save the changes as a Quick Setup when you exit. If you have changed only Hardware node or Instrument node settings, the software does not prompt you to save changes when you exit. Use the button to save these changes to a Quick Setup
Use the following buttons to manage your quick setups.
Saves the current software configuration as a Quick Setup. Enter a name
for your setup in the
window
that appears.
To save only Hardware parameter changes, you must use the button. You are not prompted to save Hardware parameter changes when closing or exiting the software unless changes are also made to the Waveform Setup.
Opens the selected Quick Setup.
Deletes the selected Quick Setup from the list. Confirm or cancel the
deletion in the
window
that appears.
You cannot delete any of the factory default Quick Setups.
Allows you to change the name of the selected Quick Qetup.
You cannot rename any of the factory default Quick Setups.