The following example procedure shows how to create Bluetooth low energy wireless technology packets.
Select from the Format in the menu bar.
Click in the navigation tree on the left to ensure that the states for (or ) and are set to On.
Click in the tree view on the left to configure the packet parameters.
Set to .
Change to .
Click the
in the tool bar to generate and download the waveform to the
signal generator.