Clicking Instrument in the
tree view
displays the Instrument settings table in the node view of the main
window.
Click the plus
box to expand the table and access those
parameters.
Press this button to send the software parameters to the connected instrument.
Press this button to retrieve the parameters from the connected instrument.
Press this button to deactivate remote operation and return the signal generator to local (front panel) control.
Press this button to set the signal generator to a known state, either factory-defined or user-defined.
Refer to the signal generator's user's guide for information on setting a user-defined state.
Press this button to execute an I/Q DC Calibration to minimize errors associated with offset voltages.
DC Cal minimizes I/Q offset errors for a single frequency only, and must be repeated if the signal generator's settings change.
Download a waveform to set the correct parameters for the target instrument, and make this button available.
Press this button to execute a manual power search calibration.
This is an internal calibration routine that improves output power accuracy when ALC is off. A power search is recommended for pulse-modulated signals with pulse-widths less than two microseconds.
Download a waveform to set the correct parameters for the target instrument, and set ALC to Off to make this button available.