FCC

1. Basic 2. Signal Configuration

Trial IDs

Pulse Width

Number of Trials

PRI

Interval Between Trials

Number of Pulses per Burst

Radar Type

Number of Bursts

Standard Version

Chirp Width

UUT Channel Center Frequency

Frequency Hopping Range

UUT Occupied Bandwidth

 

Radar Detection Bandwidth

 

1. Basic

Trial IDs

Displays the trial ID range included in the current FCC radar profile.

Number of Trials

Range: 1 to 200

Default: 30

Enter the number of trials to generate.

Interval Between Trials

Range: 0.0 ~ 600.0 s

Default: 0.0 s

Set the interval time between trials.

Radar Type

Choices: Type 0 |Type 1 | Type 2 | Type 3 | Type 4 | Type 5 | Type 6

Default: Type 1

Coupling: Type 0 is only viable when Standard Version under DFS node is set to FCC-13-22.

Select a radar type of FCC radar profiles. For the detailed description of each type, refer to FCC Radar Profiles.

If there are other FCC radar profiles with type 0~ type 4 in the trial list setting table under DFS node, type 5 and type 6 cannot be selected and a message will be displayed on the status bar "Just type 0~4 signals can be mixed. To configure type 5 or type 6 signal, please remove all the current signals firstly".

If there are other FCC radar profiles with type 5 or type 6 in the trial list setting table under DFS node, other radar types cannot be selected and a message will be displayed on the status bar "Just type 0~4 signals can be mixed. To configure other signals, please remove all the current type 5/type 6 signals firstly".

Standard Version

This cell displays the standard version under use. It is real-only and coupled to the Standard Version settings under DFS node in the tree view. Refer to FCC 06-96 and FCC 13-22 for more details about the definition of the radar profiles.

UUT Channel Center Frequency

Range: 5 GHz ~ 6 GHz

Default: 5.5 GHz

Coupling: This cell is only visible when the FCC Standard Version is set FCC-13-22 and the Radar Type is set to Type 5.

Set the UUT channel center frequency for FCC type 5 signal according to 905462 D02 UNII DFS Compliance Procedures New Rules v02.

UUT Occupied Bandwidth

Range: 5 MHz ~ 160 MHz

Default: 5 MHz

Coupling: This cell is only visible when the FCC Standard Version is set FCC-13-22 and the Radar Type is set to Type 5.

Set the UUT occupied bandwidth for FCC type 5 signal according to 905462 D02 UNII DFS Compliance Procedures New Rules v02.

Radar Detection Bandwidth

Range: 1 MHz to the maximum bandwidth determined by the connected instrument

Default: Maximum bandwidth determined by the connected instrument

Coupling: This cell is only visible when the FCC Standard Version is set FCC-13-22 and the Radar Type is set to Type 6.

Enter the radar detection bandwidth so that it is equal to the operating bandwidth of the WLAN device. Only the hopping points within the frequency band (formed by center frequency and radar detection bandwidth) will actually be transmitted by the instrument. Refer to Simulated Frequency Hopping Generation for more details.

The maximum value is determined by the sampling clock of the connected instrument, which is Max Sample Clock X 0.8.

2. Signal Configuration

Pulse Width

Displays the pulse width.If the pulse width of the selected radar type is a range instead of a fixed value, another three parameters will be displayed under this cell, step, min, and max.

Step

Displays the resolution of random value selection.

Min

Displays the lower limit of the range.

Max

Displays the upper limit of the range.

PRI

Displays the Pulse Repetition Interval (PRI) value. If the PRI of the selected radar type is a range instead of a fixed value, another three parameters will be displayed under this cell, step, min, and max.

Step

Displays the resolution of random value selection.

Min

Displays the lower limit of the range.

Max

Displays the upper limit of the range.

Number of Pulses per Burst

Displays the number of pulses per burst. If the number of pulses per burst value of the selected radar type is a range instead of a fixed value, another three parameters will be displayed under this cell, step, min, and max.

Step

Displays the resolution of random value selection.

Min

Displays the lower limit of the range.

Max

Displays the upper limit of the range.

Number of Bursts

Displays the number of bursts in the radar signal. If the number of bursts value of the selected radar type is a range instead of a fixed value, another three parameters will be displayed under this cell, step, min, and max.

Step

Displays the resolution of random value selection.

Min

Displays the lower limit of the range.

Max

Displays the upper limit of the range

Chirp Width

This cell is only visible when Radar Type is set to type 5 and it displays the bandwidth of the chirp radar signal. As it is a range as defined in the standard, there are three other parameters under it, step, min, and max.

Step

Displays the resolution of random value selection.

Min

Displays the lower limit of the range.

Max

Displays the upper limit of the range.

Frequency Hopping Range

This cell is only visible when Radar Type is set to type 6. It displays the frequency band of the frequency hopping. As the frequency band is a range, there are three other parameters under it, step, min, and max.

Step

Displays the resolution of random value selection.

Min

Displays the lower limit of the range.

Max

Displays the upper limit of the range.