Click in the tree view to display the window shown below.
Displays the licensed feature's index number.
Double-click or use the drop-down menu to set the operating state of the selected feature.
The State cell turns red if a feature is set to and a valid license is not available.
If you set the state to for a licensed feature that is used in the current setup, a window appears that enables you to save the current setup before continuing.
Displays the model number of the licensed feature.
Displays a description of the licensed feature.
Displays the status of the selected license on the connected instrument.
– the license is installed and active.
– the license is expired or not installed.
– the license is not applicable.
– The Signal Studio software does not provide license information for 16800/16900 logic analyzers and the N5343A DigRF solution.
When a new instrument connection is established or the hardware configuration is changed, the instrument licenses are automatically retrieved from the connected instrument. If the connected instrument does not have the correct licensing for the current waveform setup, initial settings are restored. You are prompted to save the setup parameters before continuing.
Displays the name of the carrier associated with the selected feature.
Displays the status of the carrier.
– the carrier is available for use.
– the carrier is not available or the license is not active.
Displays the name of the feature required for the selected carrier.