Import an SCMA settings file in CSV format.
Export an SCMA settings file in CSV format.
Range: 1 to 16
Default: 6
Set the number of layers for SCMA.
Default: 4
Range: 2 to 64
Set the codeword size for SCMA.
Range: 1 to 16
Default: 4
Set the spreading factor for SCMA.
Displays the SCMA layer index.
Enable or disable the current SCMA layer.
Choices: PN9 | PN15 | PN23 | Custom Bit Pattern | User File
Default: PN9
Opens the
Data Setup editor to configure payload bits.You can also load, save, and create custom bit patterns.
PN Seed is in hexadecimal format and is applicable only to PN types (PN9, PN15, and PN23).
Offset is in decimal format and is applicable to all data types (including PN9, PN15, PN23, custom pattern, and user file).
PN Seed and Offset require license version 2024.0801 or later.
Range: 0 to 1000
Default: 0
Set the data offset of the payload data.
Displays the codebook for the currently selected layer, allowing you to directly edit complex resource element values.
Shows the constellation for current selected layer.
Shows all codebooks. Red indicates the layer is enabled. Gray indicates the layer is disabled.
Shows the relationship between layer and resource element. Red indicates the layer is enabled. Gray indicates the layer is disabled.