The Custom IQ Type: APSK & PSK & QAM waveform setup allows you to configure a frame with multiple data segments and/or idle segments. For each data segment, the modulation type can be further configured using a graphical constellation settings editor.
Use this
drop-down menu to select a modulation type from several supported formats. A single data segment using that modulation type appears in the segment list below. Click the cell in the Constellation column to open the Constellation Setting window, providing a graphical display and editing features (video). Quick setups enable you to configure complex signals for signal generation, equivalent to 89600B VSA setups in signal analysis.
Quick Setups IQ Settings
|
Standard |
Modulation |
Symbol Rate |
Filter |
|
|---|---|---|---|---|
|
APCO25 |
C4FM |
4FSK (0.6 kHz, 1.8 kHz, -0.6 kHz, -1.8 kHz) |
4.8 ksps |
NYQ (0.2) + 1/Sinc |
|
CQPSK* |
Pi/4 DQPSK |
4.8 ksps |
NYQ |
|
|
HCPM |
4FSK (1 kHz, 3 kHz, -1 kHz, -3 kHz) |
6 ksps |
APCO25 HCPM |
|
|
HDQPSK |
Pi/4 DQPSK |
6 ksps |
APCO25 HDQPSK |
|
|
TETRA |
Pi/4 DQPSK |
18 ksps |
RNYQ (0.35) |
|
|
NXDN |
4800 bps |
4FSK (0.35 kHz, 1.05 kHz, -0.35 kHz, -1.05 kHz) |
2.4 ksps |
RNYQ (0.2) + Sinc |
|
9600 bps |
4FSK (0.8 kHz, 2.4 kHz, -0.8 kHz, 2.4 kHz) |
4.8 ksps |
RNYQ (0.2) + Sinc |
|
|
dPMR |
4FSK (0.35 kHz, 1.05 kHz, -0.35 kHz, -1.05 kHz) |
2.4 ksps |
RNYQ (0.2) |
|
|
DECT |
2FSK (-288 kHz, 288 kHz) |
1.152 Msps |
Gaussian (0.5) |
|
|
DMR |
4FSK (0.648 kHz, 1.944 kHz, -0.648 kHz, -1.944 kHz) |
4.8 ksps |
RNYQ (0.2) |
|
| ARIB |
T98/T61* |
Pi/4 DQPSK |
9.6 ksps |
RNYQ (0.2) |
|
T102 |
4FSK (0.33 kHz, 0.99 kHz, -0.33 kHz, -0.99 kHz) |
4.8 ksps |
ARIB T102 RNYQ (0.2) + Gaussian (0.769) |
|
|
Zigbee |
BPSK |
BPSK |
600 ksps |
NYQ (1) |
|
OQPSK |
OQPSK |
1 Msps |
Half Sine |
|
|
WiSUN |
2FSK 50/1 |
2FSK (-25 kHz, 25 kHz) |
50 ksps |
Gaussian (0.5) |
|
2FSK 100/0.5 |
2FSK (-25 kHz, 25 kHz) |
100 ksps |
Gaussian (0.5) |
|
|
ITU-T G.9959 |
R2 |
2FSK (-20 kHz, 20 kHz) |
40 ksps |
Rectangle |
|
R3 |
2FSK (-29 kHz, 29 kHz) |
100 ksps |
Gaussian (0.6) |
|
* For APCO25 CQPSK and ARIB T98/T61, the ALC is set to off to achieve better EVM. For all other cases, the ALC is on.
Payload, Idle Interval, Ramp Symbols, and Number of Symbols will be set to default values.
This feature saves the Custom IQ configuration as an 89600B VSA setup file, making it easier to configure complex constellations, such as 256APSK.
VSA software must be version 18.0 or later to support Custom IQ demodulation. If there is more than one data segment configured in the list, only the selected data segment (indicated by the graphical display at the bottom) will be saved to the VSA setup file. Idle segments cannot be saved to the setup file.
Differential and offset modulation types (e.g. pi/4 DQPSK or OQPSK) are found under DigitalDemod on the VSA.
The VSA does not support the APCO25 HDQPSK filter.
FSK configurations are found under DigitalDemod on the VSA.
The VSA does not support ARIB T102 and NXDN filters.
For added convenience, you can save the VSA setup as a quick setup in the VSA's Custom IQ Demod Property window. To do this, recall the Signal Studio VSA setup file, perform the measurement, and then click . Now, whenever you click , you will find your previously saved setup listed among the other setups provided with the VSA software. Using this method, you no longer need to recall the Signal Studio VSA setup file each time you want to perform a measurement.
Choices: ASK & PSK & QAM | FSK | SOQPSK | ARTM Multi-h CPM
Default: ASK & PSK & QAM
Select the type of Custom IQ.
Range: 1 kSa/s to 4 GSa/s
Default: 1 MSa/s
Sets the symbol rage of the waveform.
Choices: Low Pass| Gaussian | Root Nyquist | Nyquist | Rectangle | User Defined
Default: Root Nyquist
Select the filter type to be applied to the waveform.
Range: 0.01 to 1.0
Default: 0.5
Sets the alpha factor of the Root Nyquist or Nyquist filter.
Opens a
Filter Editor window where you can import, export, and edit filter coefficients. A convenient plot of the filter's impulse response is displayed and updates as coefficients are changed. Imported and exported coefficient files are in text (*.txt) or comma-separated values (*.csv) format.
Range: 1 kHz to Sample Rate
Default: 1 MHz
Sets the bandwidth for a low-pass filter.
Range: 0.1 to 1.0
Default: 0.5
Sets the BT product of the Gaussian filter.
Range: 1 to 1000
Default: 32
Sets the length of the filter in symbols.
Choices: Data Segment | Idle Segment
Adds a segment row to the end of the segment table. Choose between data and idle segments.
Removes the selected segment row from the segment table.
Moves the selected segment row up one position in the segment table.
Moves the selected segment row down one position in the segment table.
Sets the name of the segment. Click on the name to edit.
Displays the segment type: DATA or IDLE.
Range: 1 to 100000
Default: 1000
Sets the length of the segment in number of modulated symbols. The total number of symbols should be greater than the length of filter.
Choices: PN9 | PN15 | PN23 | Custom Bit Pattern | User File
Default: PN9
Opens the
Data Setup editor to configure payload bits.You can also load, save, and create custom bit patterns.
Choices: BPSK | QPSK | 8PSK | 16QAM | 32QAM | 64QAM | 128QAM | 256QAM | 512QAM | 1024QAM | 2048QAM | 4096QAM | User defined
Default: 16QAM
Displays the modulation type for the segment. Click the cell to open the Constellation Setting window where you can customize the consellation.
Range: 0 to 360
Default: 0
Set an additional phase rotation applied to the constellation for the segment. To view the phase rotation, you can check the checkbox in the Constellation Setting window.
Enable or disable shift for phase rotation. When enabled, the phase rotation is only applied to the odd symbol. For example: pi/2 shift BPSK, pi/4 shift QPSK. When shift is enabled, differential and offset are disabled and set to false. When differential or offset is enabled, shift is disabled and set to false.
Displays the number of bits contained in one modulated symbol.
Enable or disable the differential encoding for the segment. This can be enabled only for BPSK, QPSK, and 8PSK constellations. Differential and Offset modes cannot be enabled simultaneously.
Enable or disable IQ offset by half symbol time. This can only be enabled for a QPSK constellation. Differential and Offset modes cannot be enabled simultaneously.