Real Time

Interface Problems

If you experience problems communicating with or controlling instruments over the LAN or GPIB, check the following items. If this does not solve the problem, refer to the Connection Expert utility installed with the Keysight IO Libraries. For more information about using Connection Expert, see the Keysight IO Libraries Suite online help.

Troubleshooting the GPIB Interface

  1. Inspect the cable and connectors; confirm that none are damaged.

  2. Ensure that the GPIB cable is securely connected to the PC and the instrument.

  3. Verify that the instrument is turned on.

  4. To verify that the GPIB address entered in the software matches that of the instrument, select Hardware in the software's tree view.

  5. Validate the connection.

    1. Select Hardware in the software's tree view and click Test I/O Connection.

    2. Read the messages in the Result and Note cells to verify that the software is connecting to the instrument.

  6. Review the information about installing Keysight I/O libraries

Troubleshooting the LAN Interface

If the instrument is connected directly to a computer, use a crossover LAN cable; if the instrument is connected to a network/external server, use a standard LAN cable. 

  1. Inspect the cable and connectors and replace if damaged.

  2. Ensure that the LAN cable is securely connected to the PC and the instrument.

  3. Ensure that the instrument LAN connectors are active: flashing green or yellow lights indicate LAN activity.

  4. To verify that the Hostname or IP address entered in the software matches that of the instrument, select Hardware in the software's tree view.

  5. Validate the connection.

    1. Select Hardware in the software's tree view and click Test I/O Connection.

    2. Read the messages in the Result and Note cells to verify that the software is connecting to the instrument.

  6. Run the 'ping' program:

    1. On the computer go to Start > Programs > Accessories > Command Prompt (or DOS).

    2. At the C:\> prompt, enter ping <IP address>, where <IP address> is the instrument's IP address or hostname.

    3. If the instrument does not respond, contact your IT department for help.

  7. If the PC is connected directly to the instrument (using a cross-over cable) and the 'ping' program works correctly, but there is still a connection problem, add the instrument's IP address and hostname to the Hosts file, which resides at: C:\Winnt\system32\drivers\etc\Hosts.

    1. In a text editor such as Notepad, open the Hosts file.

    2. Write the IP address and hostname of the instrument at the bottom of the file.

      (Refer to the example of a hosts file below.)

    3. Save the file and close the text editor.

Do not use "Save As" when saving the Hosts file; this file does not have a file extension.

Example Hosts File 

# Copyright (c) 1993-1999 Microsoft Corp.

#

# This is a sample HOSTS file used by Microsoft TCP/IP for Windows.

#

# This file contains the mappings of IP addresses to host names. Each

# entry should be kept on an individual line. The IP address should

# be placed in the first column followed by the corresponding host name.

# The IP address and the host name should be separated by at least one

# space.

#

# Additionally, comments (such as these) may be inserted on individual

# lines or following the machine name denoted by a '#' symbol.

#

# For example:

#

# 102.54.94.97 rhino.acme.com # source server      

# 38.25.63.10 x.acme.com # x client host         

<xxx.xxx.xxx.xxx> localhost

<xxx.xxx.xxx.xxx> <signal generator hostname>

Software Problems

Instrument Problems

Equipment Setup and Connection