Choices: Sinc | User Defined
Default: Sinc
Select the filter type applied to F-OFDM subband.
Display the oversampling ratio of the waveform.
Display the sample frequency of the F-OFDM waveform.
Range: 1 to 2048
Default: 32
Set the length of the filter in symbols.
Set the cutoff frequency of the filter in Hz.
The resulting filter bandwidth should not be less than the subband bandwidth.
Choices: Hanning | Hamming | Rectangle
Default: Hanning
Select the window type applied to the filter.
Select the file that contains user filter coefficients. This parameter appears only when User Defined is selected as the Filter Type.
Displays the impulse response of the filter.
Displays the frequency response of the filter.