Real Time

Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

UFMC Subband Filter Editor

UFMC Filter Setting

Filter Type

Choices: Chebyshev window | User Defined

Default: Chebyshev window

Select the UFMC Filter Type.

Oversampling Ratio

Display the oversampling ratio (same as the one under Waveform Setup node).

Length (symbol)

Range: 1 to 1000

Default: 16

Set the length of the filter in symbols.

Sidelobe Attenuation

Range: 0 to 200

Default: 120

Set the sidelobe attenuation of Chebyshev window in dB.

Bandwidth (-3db)

Display the normalized 3 dB bandwidth of filter and the number of subcarriers covered.

Filter Coefficient

Select the file that contains user filter coefficients. This parameter appears only when User Defined is selected as the Filter Type.

Impulse Response

Displays the impulse response of the filter.

Frequency Response

Displays the frequency response of the filter.