The N7609B Signal Studio for Global Navigation Satellite Systems software can be used in two different configurations:
The software can be installed on a PC for use with the N5172B EXG or N5182B MXG X-series signal generators. The PC software allows the user to configure settings, generates scenario data, and provides a user interface for real-time control of the signals being produced by the signal generators.
The software can be used with the N5106A PXB baseband generator and channel emulator to create baseband GNSS signals, which are upconverted to RF using an N5172B EXG, N5182A/B MXG, or E4438C ESG signal generator. The software is already installed as a component of the PXB firmware. However, to use the software, you must purchase and install a license, and ensure that the PXB and signal generator meet the minimum hardware requirements.
|
N5172B EXG X-Series RF vector signal generator |
Firmware: Version B.01.30 or later (how to upgrade) Required options: N5172B-503 (9 kHz to 3 GHz frequency range) N5172B-653 (Internal baseband generator, 32 MSa/sec, up to 60 MHz RF bandwidth) N5172B-660 (upgrade baseband generator with real-time capability) Recommended options: N5172B-009 (internal Flash drive) N5172B-403 (calibrated AWGN for testing with noise) N5172B-660 is not required for the N7609B software's basic option. When the N5172B EXG is used solely for RF upconversion with the PXB, the only required option is N5172B-503 |
|
N5182B MXG X-Series RF vector signal generator |
Firmware: Version B.01.30 or later (how to upgrade) Required options: N5182B-503 (9 kHz to 3 GHz frequency range) N5182B-656 (Internal baseband generator, 32 MSa/sec, up to 80 MHz RF bandwidth) N5182B-660 (upgrade baseband generator with real-time capability) Recommended options: N5182B-009 (internal Flash drive) N5182B-1EQ (low power output for Rx testing) N5182B-403 (calibrated AWGN for testing with noise) N5182B-UNX (low phase noise) N5182B-660 is not required for the N7609B software's basic option. When the N5182B MXG is used solely for RF upconversion with the PXB, the only required option is N5182B-503 |
|
N5106A baseband generator and channel emulator |
Firmware: Version A.01.60 or later (how to upgrade) Required options: N5106A-611 (1 DSP block on 1 baseband card) N5106A-632 (2 I/O ports - 2 analog I/Q out and 2 digital I/O on 1 I/O cards) N5106A-EFP (Baseband generation) Recommended options: N5106A-JFP (Calibrated AWGN) |
|
N5182A MXG vector signal generator |
Firmware: Version A.01.44 or later (how to upgrade) Required options: N5182A-503 (100 kHz to 3 GHz frequency range) N5182A-651 (30 MSa/s internal baseband generator with 8 MSa memory) Recommended options: N5182A-403 (calibrated AWGN for testing with noise) N5182A-1EL (differential I/Q outputs) N5182A-1EQ (low power < -110 dBm) When the N5182A MXG is used solely for RF upconversion with the PXB, the only required option is N5182A-503 |
|
E4438C ESG vector signal generator |
Firmware: Version C.05.23 or later (how to upgrade) Required options: E4438C-403 (calibrated AWGN for testing with noise) E4438C-503 (250 kHz to 3 GHz frequency range) E4438C-601 (Internal baseband generator, 8 MSa memory for digital bus capability) Recommended options: E4438C-UNJ (Enhanced Phase Noise) When the E4438C ESG is used solely for RF upconversion with the PXB, the only required option is E4438C-503 |
|
E8267D PSG vector signal generator |
Firmware: Version C.04.85 or later (how to upgrade) Required options: E8267D-520 (250 kHz to 20 GHz frequency range) E8267D-602 (internal baseband generator with 64 Msample memory and digital bus capability) Recommended options: E8267D-005 (6 GB internal hard drive) E8267D-403 (calibrated noise personality, required for C/N capability) E8267D-UNR (enhanced phase noise performance) |
|
E6607A/B/C EXT wireless communications test set |
Required options: E6607A-503 (3 GHz) or E6607B/C-504 (3.8 GHz) |
|
M9381A PXIe vector signal generator |
Driver: Version 1.4.400.0 or later Required options: M9381A-F03, frequency range 1 MHz to 3 GHz M9381A-B04, modulation bandwidth 40 MHz M9381A-M01, 32 MSa of memory M9381A-300, adds M9300A PXIe frequency reference (if one is not already in the system) Limitations: The M9381A VSG has a limitation related to the Power Search and DC Cal functions, creating a time-synchronization loss. That is, the signal timing changes after a Power Search or DC Cal. When ALC is set to Off, Signal Studio automatically runs Power Search, which affects the user's trigger signal for starting waveform playback. Even though the timing alignment of the trigger signal and waveform are properly set, the Power Search function disrupts this synchronization. In these cases, use the following workarounds:
For DC Cal, run it before you download and play the waveform. Do not run DC Cal while the signal is playing, which disrupts the synchronization. |
|
E6640A EXM wireless test set |
Software: Version E.16.06 or later Recommended options: E6640A-B85 (increases signal bandwidth to 80 MHz) E6640A-B1X (increases signal bandwidth to 160 MHz) |
200 GB HDD with 2 GB free disk space at runtime (5 GB or higher recommended)
1024 x 768 screen resolution (1280 x 1024 recommended)
Windows 8.1 (Pro/Enterprise) (32/64 bit)1,2:
1 GHz or faster 32-bit or 64-bit processor
1 GB of memory minimum for the 32-bit version
2 GB of memory minimum for a 64-bit version
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer (8.0 or later)
Microsoft .NET Framework 3.5 or .NET Framework 3.5 Service Pack 1 (2. Downloading and Installing the .NET Framework)
Keysight IO Libraries, version 17.1 or later (3. Downloading and Installing the Keysight IO Libraries Suite)
Keysight License Manager (4. Downloading and Installing the Keysight License Manager )
128 MB graphics memory with DirectX 9 graphics support (recommended)
Windows 7 (Professional/Ultimate/Enterprise)1,2:
1 GHz or faster 32-bit or 64-bit processor
1 GB of memory minimum for the 32-bit version
2 GB of memory minimum for a 64-bit version
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer (8.0 or later)
Microsoft .NET Framework 3.5 or .NET Framework 3.5 Service Pack 1 (included with Windows 7) (2. Downloading and Installing the .NET Framework)
Keysight IO Libraries, version 17.1 or later (3. Downloading and Installing the Keysight IO Libraries Suite)
Keysight License Manager (4. Downloading and Installing the Keysight License Manager )
128 MB graphics memory with DirectX 9 graphics support (recommended)
Installed GPIB IO interface card, LAN interface card, or USB/GPIB interface connector
Keysight VISA
Microsoft Windows Installer version 2.0 or later
1 No support for Itanium64.
2 Signal Studio is compatible with the 64-bit operating system, but performs at the 32-bit speed.