The settings in this topic are available only with the Capability property selection of Advanced Real-time Signal Generation found in the GNSS node.
Choices: Start | Pulse per second | Pulse per millisecond
Default: Marker 1--Start, Marker 3--Pulse per second, Marker 4--Pulse per millisecond
Select the signal pattern for the marker output. The marker output signal is mapped to a rear panel connector on the signal generator.
On an ESG:
Marker 1 correlates to the EVENT1 output connector and the AUX IO connector
Marker 3 and Marker 4 correlate to only the AUX IO connector
On an EXG/MXG, all three marker signals are available at the rear panel AUX IO connector, or use the front panel to route two of the marker signals to the following rear panel connectors (one signal per connector):
EVENT 1 (marker 1 is the default setting for this connector)
TRIG OUT
To access the rear panel connector routing selections from the front panel, use the following hardkey and softkeys: Mode > Real-Time Applications > Real-Time Apps System Settings > Route to Baseband BNCs.
For more information on the signal generator rear-panel connectors and marker output signals, see the signal generator's User Guide.
EXG/MXG:
[:SOURce]:RADio:GNSS[:BBG]:MARKer[1]|3|4]:APRovided:TYPE STARt|MS|PPS
[:SOURce]:RADio:GNSS[:BBG]:MARKer[1]|3|4]:APRovided:TYPE?
Range: …–1 ms to 1 ms (resolution of 15 ns)
Default: 0 ns
Enter an offset value to apply dynamic timing adjustment to and markers. A positive value means timing delay and a negative value means timing advance. Hardware supported timing adjustment resolution is 8 ns.
EXG/MXG: