Use this process to convert a Google Earth kml file to an NMEA GGA file for use by the scenario generator.
Start Google Earth on your PC.
Use the Google Earth tool to create the trajectory.
On the tree node, right click the path you created and select to save the file as a kml file.
If playing a scenario, click the button.
In the tree node, select .
Click the tab.
Click
Convert KML to launch the dialog box.
On the dialog box:
Click to launch the dialog box to navigate to and open the saved Google Earth kml file.
After selecting the kml file, the file path and name appears to the right of the button..
If desired, change the file properties for the conversion.
Click the button to launch the dialog box for selecting a location and saving the file as an NMEA GGA file type.
After saving the converted NMEA GGA file, click the
to close the dialog box.
Click the tab.
Click the cell and use the drop-down arrow to select .
With the selection, the cell appears .
Click the cell, and use the dialog box button
to launch the dialog box for navigating
to and selecting the converted NMEA message file.
After selecting the file, the cell automatically updates to the date of 2010-01-01 and the time from the KML to NMEA Converter, Start Time property.
The start time in the scenario generator uses GPS time versus UTC time for the Start Time property of the KML to NMEA Converter. Because of the different time types, the scenario generator start time will always show 15 leap seconds later than the KML to NMEA Converter, Start Time property.
Change the date of the cell to match the date of the almanac file.
For the factory supplied almanac files, the date is part of the file name or you can view these almanac file dates in the Factory Supplied GNSS Files topic.
Do change the time, change only the date. The software uses the first time found in the GGA file.