The Scenario Graphics tab is divided into two parts: a graphic panel on the top and generation log window at the bottom. The graphics panel displays the content of the selected scenario, where each constellation is represented by a different color. The left side of each channel bar displays the SV ID, which is coded with a constellation prefix of:
G = GPS
R = GLONASS
E = Galileo
B = Beidou
Black space on a channel bar indicates that no signal is transmitted on the channel for that period. The time axis of the scenario is displayed at the bottom of channel bars. The content of the graphic panel is updated whenever a new scenario file is created or a scenario file is selected for the editing.
The generation log window provides the information on the scenario generation process, including scenario header, generation results, warnings and errors. Whenever you click the 'Create Scenario', 'Save Scenario' or 'Apply' buttons, or load a new scenario for editing, new messages will be appended to log window. You can use these messages for troubleshooting, for example, to verify correct input parameters.